cancel
Showing results for 
Search instead for 
Did you mean: 

Find a way to communicate some event that the network recognizes and sent it out of panel stm32h747i

wjian.2
Associate III

If i want to send the result of (Food-Recognition)of FP-AI-VISION1_V3.1.0,to achieve to object of  to communicate some event that the network recognizes (for example the detection of a certain object) and send it out of the panel.The complete project is shown: development board + external board (raspberry or arduino or whatever).

Hay some software o method o project to achieve this?

0 REPLIES 0