cancel
Showing results for 
Search instead for 
Did you mean: 

error when analyzing the .onnx model in stm32cubeMX by stm32cube.AI

BHuan.3
Associate III

Hi, Thanks for your attention. I am analyzing the .onnx format model but an error occurs. I try to reinstall the stm32cubeMX but it doesn't help.

0693W00000QKl99QAD.pngThe part of architecture is:

0693W00000QKlBZQA1.png 

Here is the log information. Can you help me with this problem? @Romain LE DONGE​  @jean-michel.d​ @fauvarque.daniel​  Thanks very much!

2022-07-08 15:39:51,314 [INFO] BoardInfo:879 - No configuration file found for board P-NUCLEO-WB55
2022-07-08 15:39:51,316 [INFO] DbBoards:156 - Kit is not supported: P-NUCLEO-WB55
2022-07-08 15:39:51,319 [INFO] BoardInfo:879 - No configuration file found for board STEVAL-BFA001V1B
2022-07-08 15:39:51,320 [INFO] DbBoards:156 - Kit is not supported: STEVAL-BFA001V1B
2022-07-08 15:39:51,321 [INFO] BoardInfo:879 - No configuration file found for board STEVAL-BFA001V2B
2022-07-08 15:39:51,321 [INFO] DbBoards:156 - Kit is not supported: STEVAL-BFA001V2B
2022-07-08 15:39:51,404 [INFO] DbBoards:160 - Found 176 boards, 173 are supported
2022-07-08 15:39:51,408 [INFO] ApiDb:418 - Load user favorites file /Users/name/.stm32cubemx/favorites.boards.txt: 0 item(s)
2022-07-08 15:39:51,408 [INFO] ApiDb:422 - User favorites Boards=[]
2022-07-08 15:39:51,409 [INFO] DbBoards:189 - Set 0 / 0 favorites Boards
2022-07-08 15:39:56,930 [INFO] ExtendedFilter:65 - Artificial Intelligence: enable filter
2022-07-08 15:39:56,938 [INFO] McuExtendedFiltersManager:86 - Reset MCU extended filter: Artificial Intelligence
2022-07-08 15:40:11,418 [INFO] AInterface:235 - ModelName:network; files:[/Users/name/STM32Cube/test.onnx]; type:ONNX; compression:None
2022-07-08 15:40:11,434 [INFO] AInterface:515 - workspaceTempDir: /var/folders/y8/7c4vvzbj2l1dw7trnz05b52m0000gn/T/mxAI_workspace5038345178307913369027895421033696
2022-07-08 15:40:11,438 [INFO] AInterface:1065 - Setting Env: /Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac
2022-07-08 15:40:11,440 [INFO] AInterface:1122 - Custom PATH variable: /Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac:/bin:/usr/bin:/usr/sbin:/sbin:/Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac/node/bin
2022-07-08 15:40:11,500 [INFO] CmdLine:100 - Command: /Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac/stm32ai analyze --name network -m /Users/name/STM32Cube/test.onnx --type onnx --compression none --verbosity 1 --workspace /var/folders/y8/7c4vvzbj2l1dw7trnz05b52m0000gn/T/mxAI_workspace5038345178307913369027895421033696 --output /Users/name/.stm32cubemx/network_output --allocate-outputs
2022-07-08 15:40:12,022 [INFO] CmdLine:132 - stm32ai exit with status: 132
2022-07-08 15:40:12,025 [ERROR] CmdLine:135 - stm32ai return with an error

9 REPLIES 9
BHuan.3
Associate III

@VTOMA.1​ 

BHuan.3
Associate III

I have checked that all the layers in my .onnx model are supported.

Please refer to ..../STM32Cube/Repository/Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Documentation/supported_ops_onnx.html

fauvarque.daniel
ST Employee

Do you have the same error when running the stm32ai command by hand in a terminal window ?

just type

/Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac/stm32ai analyze /Users/name/STM32Cube/test.onnx

Regards

Daniel

Dear fauvarque.daniel @fauvarque.daniel​ ,

Thanks for your quick reply. I try the follow exec command but get the error: illegal hardware instruction. I am using an M1 pro chip in Macbook pro 14inch.

/Users/name/STM32Cube/Repository//Packs/STMicroelectronics/X-CUBE-AI/7.2.0/Utilities/mac/stm32ai analyze /Users/name/STM32Cube/test.onnx

There is the same question unsolved here.

https://community.st.com/s/question/0D53W00001dwl1GSAQ/stm32ai-illegal-hardware-instruction-on-mac-m1

Looking forward to your reply.

The current generation for Mac is done for x86 based mac assuming that Apple has implemented a backward compatibility with the x86 applications.

It doesn't seem to be the case, we'll have to investigate how to solve the issue (specific build for the M1 ?)

Regards

Daniel

Dear Daniel,

Thanks for your reply and help.

Yes, I think at present M1 can't work. M1 Mac needs a specific build.

There is another question related to this problem highly. Please refer to https://community.st.com/s/question/0D53W00001dwl1GSAQ/stm32ai-illegal-hardware-instruction-on-mac-m1

Looking forward to your solution. @fauvarque.daniel​ 

Best wishes,

Baichuan

Hi @BHuan.3​ 

I just replied the thread you mentioned,

Can you try enabling manually Apple's Rosetta 2 compatibility layer using the solution from this thread: https://github.com/nvm-sh/nvm/issues/2350#issuecomment-734132550

0693W00000QKq94QAD.pngThen try running again the stm32ai command line call

Hope it can help,

Regards,

Romain

@Romain LE DONGE​ 

Dear Romain,

Thanks for your quick and kind reply. I try it but fail.

That is sad news. Maybe we need a new build one for M1 specifically or use windows instead.

Best wishes,

Baichuan

eugenn
Associate

Hi @fauvarque.daniel, I have same issue on my macbook m2pro, are you planning to fix that issue?