cancel
Showing results for 
Search instead for 
Did you mean: 

X-CUBE-USB-PD install

DalOpez
Associate II

Hello. I'm trying to figure out X-CUBE-USB-PD. As I understand it, this is an extension for CubeMX, but I can't figure out how to install this extension. Downloaded the project from the link https://github.com/STMicroelectronics/x-cube-usb-pd . I was given the task to implement the functionality of the project from the example on the stm32f4 device. Please help me figure it out. For the second week I can't figure it out.

This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Guillaume K
ST Employee

The version on github doesn't seem to be an extension to CubeMX. There's no *.ioc file.

Just get all the files and run directly the IDE project files provided under Projects/ ... / EWARM, MDK-ARM or STM32CubeIDE.

DalOpez
Associate II

I have already done as you advised. CubeIDE discovered the EVAL_FUSB307_DRP project. If you do not make any changes, the project is built without problems. However , if you remove any .c or .h file, errors appear in the project. So far, they have no thoughts on how to use this project to implement power delivery on stm32f4.