2021-07-21 2:25 AM
Hello everyone,
I want to connect my STM32H747-Disco board to my AWS IoT services and the AWS S3.
I've attempted to do it with minimal changes with the aws_Demo application project from the X-CUBE-AWS V2.2.0 expansion package:
1. Compile projects in the following order. This is mandatory as each project requests some objects generated by the
compilation of the previous one:
- 2_Images_SECoreBin (see also SECoreBin/readme.txt)
- 2_Images_SBSFU
- 2_Images_UserApp (see also UserApp/readme.txt)
I couldn't understand what is the UserApp (I guessed it the aws_demo app), so I've downloaded the X-Cube-SBSFU package, and still couldn't make it boot...
Conclusion:
I could not find any STM32H747-DISCO example of those 2 packages, and couldn't make it boot (nothing on the UART console). What have I done wrong? Is it even possible to port some of those examples to the STM32H747/757 DISCO/EVAL boards?
Thanks in advance for everybody.
2021-07-30 2:42 AM
The X-CUBE-AWS V2.2.0 STM32H755 secure bootloader is mostly reused from the X-CUBE-SBSFU v2.4.0 STM32H753 bootloader, and relies on secure HW IPs which are only present in STM32H75x MCUs.
On STM32H74x MCUs, the SBSFU bootlader should be removed (skip the pre- and post-build steps of aws_demos, adapt the linker file), and disable the OTA update feature from the FreeRTOS build, which implementation is based on the SBSFU.
On other STM32H75x MCUs, it should be possible to port the SBSFU bootloader, but it will require to dig into its internal design.
2021-08-05 2:40 AM
Also if you want to use AWS S3 service it is not supported in X-CUBE-AWS. This package only does AWS IoT Core service with MQTT protocol.
2021-09-29 6:07 AM
@Guillaume K @grd Hi,
So I've skipped the pre and post build steps and have built and run the demo application for the M7 processor of the STM32H747 with the following steps:
What I've found from debugging:
I must mention that I did not understand, what should I change in the link file (besides deleting the INCLUDE lines)
I would like to ask for help from you:
Thanks in advance, it is really appriiciated.
2021-10-04 2:43 AM
@AAvda.1 , the linker file of an SBSFU-enabled user application cannot be used for a standalone application. You need to write your own.
The figure NUCLEO-H755ZI-Q mapping in single-core configuration of UM2178 highlights the memory areas that are important for the CPU1 user application, so they must be kept or relocated.
Possible starting or comparison points are the LwIP application examples in the STM32CubeH7 package, or the application code generated by the STM32CubeMX tool for your target.
If the hardfault occurs in an interruption context, it can be due to a wrong configuration of the vector table address. In system_stm32h7xx_dualcore_boot_cm4_cm7.c, SCB->VTOR must be set according to your linker file.
Regarding the OTA, removing the SBSFU from the build prevents the compilation of aws_ota_pal.c because SHARED_REGION_RAM_START is imported from the SBSFU definitions.
Depending on the toolchain, the file may have to be excluded from the build, or its reference to SBSFU commented out (the functions will not be called by the non-OTA demos anyway).
2021-10-05 4:50 AM
Hi @grd ,
First of all, thanks a lot!
Is there any training or user manual that will help me with the linker files? I am not that familiar with this.
BTW, I've disabled the unaligned access trap, then it run and worked, but there is a problem with the DHCP client, so I made it static IP but for some reason it is not working either
Would you recommend this way or better to start write a new linker file?
Thanks in advance,