cancel
Showing results for 
Search instead for 
Did you mean: 

Wrong PLL prediv calculation in LL driver when using the HSE?

Martin Rm
Associate
Posted on April 05, 2018 at 14:10

Hi,

I think there is a possible BUG in LL libraries when using the HSE.

My controller is a stm32f103t8 with an external Oszillator.

I use LL version V1.1.1.

The following function in stm32f1xx_ll_rcc.h should return the prediv factor for the PLL.

__STATIC_INLINE uint32_t LL_RCC_PLL_GetPrediv(void)

{

&sharpif defined(RCC_CFGR2_PREDIV1)

  return (uint32_t)(READ_BIT(RCC->CFGR2, RCC_CFGR2_PREDIV1));

&sharpelse

  return (uint32_t)(READ_BIT(RCC->CFGR, RCC_CFGR_PLLXTPRE));

&sharpendif /*RCC_CFGR2_PREDIV1*/

}

The problem is now that this function returns the bit value in that register, here 2^17 if set - not the factor itself

The function RCC_PLL_GetFreqDomain_SYS() in stm32f1xx_ll_rcc.c calculates the pll input frequency in that way:

...

case LL_RCC_PLLSOURCE_HSE:       /* HSE used as PLL clock source */

   pllinputfreq = HSE_VALUE / (LL_RCC_PLL_GetPrediv() + 1U);

   break;

...

The result is that the HSE_VALUE is divided by the bit position 2^17, the result is a wrong pll frequency.

The problem is that this functions is called indirect in LL_USART_Init, i2c and more. So the USART doesn't work

with the HSE in F1 LL drivers.

I think in the function LL_RCC_PLL_GetPrediv above is the shift operator missing in that way:

return (uint32_t)(READ_BIT(RCC->CFGR, RCC_CFGR_PLLXTPRE) >> RCC_CFGR_PLLXTPRE_Pos)

Or do I have missed something?

Thank You

#ll-bug #hse #stm32f1 #bug?
This discussion is locked. Please start a new topic to ask your question.
2 REPLIES 2
Imen.D
ST Employee
Posted on May 11, 2018 at 17:53

Hello

Rohrmoser.Martin

,

This issue is raised internally to the developer team, then we will keep you informed about the taken actions.

Best Regards,

Imen.

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
Imen.D
ST Employee
Posted on July 13, 2018 at 15:26

Hi 

Rohrmoser.Martin.001

,

We have reproduced this issue from our side for LL_RCC. The return value of LL_RCC_PLL_GetPrediv() was 2^17 and it should return the PREDIV factor for the PLL.

This issue will be fixed in the coming version of CubeF1.

Thanks and Best Regards,

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen