cancel
Showing results for 
Search instead for 
Did you mean: 

Why was the FreeRTOS_LowPower application example removed from the 1.3 package?

MKulp.1
Associate II
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
Imen.D
ST Employee

Hello @MKulp.1​ ,

Welcome to the STM32 Community =)

Which Cube package, please ?

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen
MKulp.1
Associate II

STM32Cube_FW_L5_V1.2.0 has it. Removed from my repository on STM32Cube_FW_L5_V1.3.0. My customer discovered what appears to be a bug, and wondering if reason for removal. Should I (as the Avnet FAE) direct customer away from this example?

Thanks,

Mike

I'am checking it internally and I will come back to you with details.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen

No, you can't use this application, as the FreeRTOS 10.2.1 does not support LowPower mode for the CM33.

The Tickless IDLE is only supported in the 10.3.1 release

https://github.com/FreeRTOS/FreeRTOS-Kernel/commit/177e79fc79b62e8301f85ed19633c8aef5ef708d

Please select the post as a "Best Answer" if it answered your question, so that this thread will marked as closed.

Imen

When your question is answered, please close this topic by clicking "Accept as Solution".
Thanks
Imen