cancel
Showing results for 
Search instead for 
Did you mean: 

Why enter the ISO in/out incomplete interrupt? STM32CubeExpansion_USBAudioStreaming_V1.0.0 UAC MCU STM32L476

gfeng
Associate

Hi all:

If I plug in USB 2.0 mode high speed port(PC recognition Windows7), ​frequently enter the ISO in/out incomplete interrupt. but if I plug in USB1.0 mode full speed port,is OK. Once enter the incomplete interrupt.record or playback, audio will be interrupted.

Has anyone encountered the same problem?

Many thanks�?

/**

 * @brief USBD_AUDIO_IsoINIncomplete

 *     handle data ISO IN Incomplete event

 * @param pdev: device instance

 * @param epnum: endpoint index

 * @retval status

 */

static uint8_t USBD_AUDIO_IsoINIncomplete (USBD_HandleTypeDef *pdev, uint8_t epnum)

{

 USBD_AUDIO_EPTypeDef  *ep;

 USBD_AUDIO_HandleTypeDef  *haudio;

 uint16_t current_sof;

 haudio = (USBD_AUDIO_HandleTypeDef*) pdev->pClassData;

 /* @TODO check if the feedback is responsible of event */

 for(int i = 1; i<USBD_AUDIO_MAX_IN_EP; i++)

 {

  ep = &haudio->ep_in[i];

  current_sof = USB_SOF_NUMBER();

  if((ep->open) && IS_ISO_IN_INCOMPLETE_EP(i,current_sof, ep->tx_rx_soffn))

  {

   epnum = i|0x80;

   USB_CLEAR_INCOMPLETE_IN_EP(epnum);

   USBD_LL_FlushEP(pdev, epnum);

   ep->tx_rx_soffn = USB_SOF_NUMBER();

#if USBD_SUPPORT_AUDIO_OUT_FEEDBACK  

   if(ep->ep_type==USBD_AUDIO_FEEDBACK_EP)

   {

USBD_LL_Transmit(pdev, 

epnum,

ep->ep_description.sync_ep->feedback_data,

ep->max_packet_length);

INFO("'");

    continue;

   }

   else

#endif /*USBD_SUPPORT_AUDIO_OUT_FEEDBACK */

   if(ep->ep_type==USBD_AUDIO_DATA_EP)

   {

    USBD_LL_Transmit(pdev, 

           epnum,

           ep->ep_description.data_ep->buf,

           ep->ep_description.data_ep->length);

INFO(":");

   }

   else

   {

    USBD_error_handler();

   }

   

  }

 }

 return 0;

}

/**

 * @brief USBD_AUDIO_IsoOutIncomplete

 *     handle data ISO OUT Incomplete event

 * @param pdev: device instance

 * @param epnum: endpoint index

 * @retval status

 */

static uint8_t USBD_AUDIO_IsoOutIncomplete (USBD_HandleTypeDef *pdev, uint8_t epnum)

{

return USBD_OK;

}

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0