cancel
Showing results for 
Search instead for 
Did you mean: 

While using USB Mass Storage Device and SD Card , at a time only One Device is detecting

Abin
Associate III

Hai All,

I am working on STM32F205VET and I have enabled USB Mass storage, SD Card and FATFS. I need to use SD card and USB mass Storage at a time, that means need to access the files.But I found that based on the 

FATFS_LinkDriver preference makes that one device in Disable mode. I am giving the Initialization function here.

 

void MX_FATFS_Init(void)
{
 
  /*## FatFS: Link the USER driver ###########################*/
 
retUSER = FATFS_LinkDriver(&USER_Driver, USERPath);
 
  /*## FatFS: Link the USBH driver ###########################*/
 
 
     retUSBH = FATFS_LinkDriver(&USBH_Driver, USERPath);
 
 
  /* USER CODE BEGIN Init */
     /*Use the first link driver for SD card and second for USB*/
  /* additional user code for init */
  /* USER CODE END Init */
}
 
Can yo
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0