2022-11-28 2:00 AM
hi, everyone!
May you have a nice day!
In en.stm32cubeg4_v1-5-0\STM32Cube_FW_G4_V1.5.0\Projects, core_cm4.h file.
I encounter the following codes:
__STATIC_INLINE void __NVIC_EnableIRQ(IRQn_Type IRQn)
{
if ((int32_t)(IRQn) >= 0)
{
__COMPILER_BARRIER();
NVIC->ISER[(((uint32_t)IRQn) >> 5UL)] = (uint32_t)(1UL << (((uint32_t)IRQn) & 0x1FUL));
__COMPILER_BARRIER();
}
}
So the questions are:
thank you for your attention!
Best wishes!
Solved! Go to Solution.
2023-10-09 10:41 AM
HI, everyone.
I think this post answers my question in detail, lets close this topic.
gcc - difference in mfence and asm volatile ("" : : : "memory") - Stack Overflow
2022-11-28 2:13 AM
Goto the definition of the function
Typically such things are designed to stop the compiler moving or optimizing code that has primary, or secondary, behavior the compiler can't understand.
Or involves a memory fencing requirement, where data needs to reach its final destination before completion. So pipeline and write buffers must complete before next instruction starts.
2022-11-28 6:02 PM
hi tesla, thank you for your answer~
here is its definition:
#define __COMPILER_BARRIER() __ASM volatile("":::"memory")
it seems conform to the following format:
asm(code : output operand list : input operand list : clobber list);
I am new to this, where should I go to find related literature or pdf ?
thank you very much!
2023-10-09 10:41 AM
HI, everyone.
I think this post answers my question in detail, lets close this topic.
gcc - difference in mfence and asm volatile ("" : : : "memory") - Stack Overflow
2023-10-09 11:46 AM
The predominant hazard with the NVIC and peripherals is that the write-buffers clearing the source of an interrupt can be slower than the interrupt tail-chaining mechanics resulting in it wanting to re-enter the IRQHandler somewhat spuriously. When you double-check the source it will have been cleared. So robust coding of the Handler is recommended.