Skip to main content
Senior
November 5, 2023
Solved

What does the STM32G474 do when powered on and it is erased?

  • November 5, 2023
  • 1 reply
  • 1257 views

I designed a product that uses the STM32G474 MCU and found that if the BOOT0 pin is left floating, the MCU randomly appears to be running wild code when power is first applied.  In my design, this could cause serious damage to the hardware.  Although, I can program the nSWBOOT0 options bit so that the external BOOT0 pin is ignored, the initial application of power will always observe this pin (i.e., this pin must be tied low to ensure that execution start from the main Flash memory). 

When the STM32G474 is initially unprogrammed, if the external BOOT0 pin is tied low and execution starts from the main Flash memory, what will the MCU be doing (e.g., executing NOPs, continually jumping to address 0, etc.)?

This topic has been closed for replies.
Best answer by waclawek.jan

> When the STM32G474 is initially unprogrammed, if the external BOOT0 pin is tied low and execution starts from the main Flash memory

At that point, there are a couple of option bits to check: BOOT_LOCK and BFB2; see AN2606 (pattern 14 applies to 'G47x).

But assuming BFB2=0 which is the default, execution starts with loading the first word from 0x0000'0000 i.e. 0xFFFF'FFFF into stack pointer, and also 0xFFFF'FFFF into PC. Then the processor attempts to fetch from that address and that leads to Lockup, i.e. repeated execution from the same address with no other outward activity.

In other words, in that case, all external pins remain in their reset state.

JW

1 reply

waclawek.jan
waclawek.janBest answer
Super User
November 5, 2023

> When the STM32G474 is initially unprogrammed, if the external BOOT0 pin is tied low and execution starts from the main Flash memory

At that point, there are a couple of option bits to check: BOOT_LOCK and BFB2; see AN2606 (pattern 14 applies to 'G47x).

But assuming BFB2=0 which is the default, execution starts with loading the first word from 0x0000'0000 i.e. 0xFFFF'FFFF into stack pointer, and also 0xFFFF'FFFF into PC. Then the processor attempts to fetch from that address and that leads to Lockup, i.e. repeated execution from the same address with no other outward activity.

In other words, in that case, all external pins remain in their reset state.

JW

Senior
November 5, 2023

Thank you!