2013-07-23 11:47 PM
Hi
void
main()
{
Set_System();
Set_USBClock();
USB_Interrupts_Config();
USB_Init();
while
(bDeviceState != CONFIGURED);
// wait until USB is configured
while
(1)
{
if
(count_out)
{
Virtual_Com_Write_Buffer(&USB_Rx_Buffer, count_out);
//Just send the received data on USB
count_out = 0;
}
}
return
0;
}
I'm using the above code from a project:
https://github.com/Harinadha/STM32_MPU9150eMPL/blob/master/main.c
This code works well on Olimex STM32-P103 board which has STM32F103RB. I'm using STM32F103RE micro & same version IAR EWARM project. I modified the project to make changes: FLASH, RAM size, device & USB_DISCONNECT related & defined constant USE_STM3210E_EVAL.But it alwaysstruck@
Line 8:while(bDeviceState != CONFIGURED);Please have a look at the USB circuit part of my board.