Virtual Com Port for STM32F103XC
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-04-07 3:44 AM
Posted on April 07, 2014 at 12:44
Hi Guys,
I Am trying to port VCP Example Project found in STM32_USB-FS-Device_Lib_V4.0.0 on STM32F103XE Eval kit. Pin Description : PA12------USBDP-------Pulled up by 1.5K Resistor. PA11------USBDM PA10------USART1_RX PA9--------USART1_TX So depending on same I modified as belowvoid Set_System(void)
{ GPIO_InitTypeDef GPIO_InitStructure; /*Set PA11,12 as IN - USB_DM,DP*/ RCC_APB2PeriphClockCmd(RCC_APB2Periph_GPIOA, ENABLE); GPIO_InitStructure.GPIO_Pin = GPIO_Pin_11 | GPIO_Pin_12; GPIO_InitStructure.GPIO_Speed = GPIO_Speed_50MHz; GPIO_InitStructure.GPIO_Mode = GPIO_Mode_AF_PP; //GPIO_InitStructure.GPIO_OType = GPIO_OType_PP; //GPIO_InitStructure.GPIO_PuPd = GPIO_PuPd_NOPULL; GPIO_Init(GPIOA, &GPIO_InitStructure); /*SET PA11,12 for USB: USB_DM,DP*/ // GPIO_PinAFConfig(GPIOA, GPIO_PinSource11, GPIO_AF_14); // GPIO_PinAFConfig(GPIOA, GPIO_PinSource12, GPIO_AF_14); } As GPIO_PinAFConfig is obsolete in latest standard peripheral library ( STM32F10x_StdPeriph_Lib_V3.5.0 ) so how can I set Pin11 and Pin12 as DM\DP ? Is there any substitute or how to configure same ?Regards,
Omji Mishra #usb-stm32
Labels:
- Labels:
-
USB
This discussion is locked. Please start a new topic to ask your question.
11 REPLIES 11
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-04-13 11:31 PM
Posted on April 14, 2014 at 08:31 Hi anyone has any clue regarding same.
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2014-04-24 2:27 PM
Posted on April 24, 2014 at 23:27
Hello,
I recently resolved an issue almost exactly like yours. My problem was that the PLL clock was not setup properly. I needed to enable the PLL clock and setup as follows:PLL Clock source = HSE (16Mhz external clock)PLL Multiplier = 3 (This creates a 48Mhz clock 3*16 = 48) You can use 4 here instead but you will need ot have the USB pre-selector set to divide by 1.5PLL Enable = TrueUSB Pre-selector = Divide by 1--Kevin
- « Previous
-
- 1
- 2
- Next »