cancel
Showing results for 
Search instead for 
Did you mean: 

Vbus +5V

FAnag
Associate

Hi

I plan to include the USB input of STM32F303 and am not willing to power up the board with the +5V of Vbus. The board will be supplied permanently with 3.3V. Is it necessary the connection of Vbus? If yes how i should connect it to the +3.3V Vdd of STM32?

Thanks

3 REPLIES 3
Uwe Bonnes
Principal III

You need VBUS to detect USB-plutg/unplug.

FAnag
Associate

Thanks.

So i should use one of the many circuits i found in Google, e.g. this with the FET that is connected among +3.3V Vdd ---> Res 1.5K----> D+ input with its gate driven by the Vbus +5V ? Is that OK?