Skip to main content
Bmora.1
Visitor II
March 27, 2022
Question

Using the STM32 USB-CDC example, using "Command" endpoint differs when used with STM32F1 vs STM32F4?

  • March 27, 2022
  • 2 replies
  • 1571 views

I've extended the USB-CDC example using Cube IDE to report serial port line state -- Ring, etc. My example works on STM32F1, however, it does NOT function correctly on STM32F4.

Here's the meat:

/* USER CODE BEGIN PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
USBD_StatusTypeDef USBD_CtlSendNotification(USBD_HandleTypeDef *pdev,
 
 uint8_t *pbuf, uint16_t len)
 
{
 
 /* Set EP0 State */
 
 //pdev->ep0_state = USBD_EP0_STATUS_IN ;
 
 pdev->ep_in[2].total_length = len;
 
 pdev->ep_in[2].rem_length = len;
 
 
 /* Start the transfer */
 
 USBD_LL_Transmit(pdev, CDC_CMD_EP, pbuf, len);
 
 
 return USBD_OK;
 
}
 
 
uint8_t CDC_Notify_FS(uint8_t linestate) {
 
 USBD_HandleTypeDef *pdev = &hUsbDeviceFS;
 
 
 USBD_CDC_HandleTypeDef *hcdc =
 
 (USBD_CDC_HandleTypeDef*) hUsbDeviceFS.pClassData;
 
 uint8_t ifalt = 0U;
 
 uint16_t status_info = 0U;
 
 uint8_t ret = USBD_OK;
 
 uint8_t dbuf[12];
 
 dbuf[0] = 0xA1; //bmRequestType TODO: Add Define for USB_SERIAL_STATE
 
 dbuf[1] = 0x20; //SERIAL_STATE
 
 
 dbuf[2] = 0x00; // wValue
 
 dbuf[3] = 0x00;
 
 
 
 dbuf[4] = 0x00; // windex (interface) TODO: pdev->dev_address ?
 
 dbuf[5] = 0x00;
 
 
 dbuf[6] = 0x02; // wlen
 
 dbuf[7] = 0x00;
 
 
 dbuf[8] = linestate & 0x7F; // linestate 7:0
 
 dbuf[9] = 0x00; // reserved 15:8
 
 
 USBD_CtlSendNotification(pdev, (uint8_t*) (void*) &dbuf, 0x0A);
 
 return ret;
 
}
 
/* USER CODE END PRIVATE_FUNCTIONS_IMPLEMENTATION */
 
 

Do I need to do any other initialization (on STM32F4) before I'm able to send a 10 byte buffer down the Interrupt-endpoint 82?

This topic has been closed for replies.

2 replies

Walid ZRELLI
Visitor II
March 28, 2022

Hello @Bmora.1​ ,

In order to allow a better analysis this issue, could you please give us more details about your problem.

Thanks in advance.

BeST Regards,

Walid

waclawek.jan
Super User
March 28, 2022

Make the dbuf array global or static.

JW