Skip to main content
Andrei Chichak
Lead
Jan 18, 2024 12:18 AM UTC
Solved

USBx CDC-ACM (VCP) not enumerating on Nucleo-L452RE

I'm trying to get a L452 to bring up a VCP under ThreadX/USBx, so I followed the instructions in:

https://community.st.com/t5/stm32-mcus/how-to-implement-the-usb-device-cdc-vcom-in-stm32-using-the/tac-p/629402#M738

It seemed pretty straight forward, it compiles, runs, creates the read and write threads, the main thread exits appropriately, but the USB device never enumerates on the bus.

Just to make sure that my board works (Nucleo with a USB-B connector wired into PA11/12, ground, and +5), I can put the processor into bootload, it comes up as a USB BOOTLOADER, and I can use CubeProg to push code. So the physical connection is okay.

I must be missing something. Is there something weird with the L4 that needs code tweaking? Can you please take a look?

I've attached the project below.

This topic has been closed for replies.
Andrei Chichak
Andrei ChichakBest answer
Lead
Jan 22, 2024 9:35 PM UTC

Apparently the issue is that the USB power never got turned on. Please see:

https://community.st.com/t5/stm32-mcus-embedded-software/stm32h573-usbx-cdc-acm-device/m-p/623032

Calling HAL_PWREx_EnableVddUSB() will fix this issue.

That is all

 

4 replies

Andrei Chichak
Lead
Jan 22, 2024 9:08 PM UTC

I was looking through the community threads about other instances of this issue on other processors and the typical fix is to adjust the PCD buffers. I tried a bunch of configurations including, my latest favourites:

/* USER CODE BEGIN app_ux_device_thread_entry */
MX_USB_PCD_Init();
HAL_PCDEx_PMAConfig(&hpcd_USB_FS , OUT , PCD_SNG_BUF, 0x18);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS , IN , PCD_SNG_BUF, 0x58);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS , USBD_CDCACM_EPIN_ADDR , PCD_SNG_BUF, 0xC0);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS , USBD_CDCACM_EPOUT_ADDR , PCD_SNG_BUF, 0x110);
HAL_PCDEx_PMAConfig(&hpcd_USB_FS , USBD_CDCACM_EPINCMD_ADDR , PCD_SNG_BUF, 0x100);
ux_dcd_stm32_initialize((ULONG)USB, (ULONG)&hpcd_USB_FS);
HAL_PCD_Start(&hpcd_USB_FS);
/* USER CODE END app_ux_device_thread_entry */

It still doesn't work, nor can I figure out where these values come from. Any hints from the FAEs at ST?

<bump>

Andrei Chichak
Andrei ChichakAuthorBest answer
Lead
Jan 22, 2024 9:35 PM UTC

Apparently the issue is that the USB power never got turned on. Please see:

https://community.st.com/t5/stm32-mcus-embedded-software/stm32h573-usbx-cdc-acm-device/m-p/623032

Calling HAL_PWREx_EnableVddUSB() will fix this issue.

That is all

 

KDJEM.1
ST Technical Moderator
Jan 23, 2024 8:18 AM UTC

Hello @Andrei Chichak ,

Thank you for bringing this issue to our attention.

I reported this issue internally.

Internal ticket number: 171432 (This is an internal tracking number and is not accessible or usable by customers).

Thank you.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.
KDJEM.1
ST Technical Moderator
Mar 22, 2024 8:07 AM UTC

Hi @Andrei Chichak ,

The issue is fixed in STM32CubeMX 6.11.0.

Thank you for your contribution in STCommunity.

Kaouthar

To give better visibility on the answered topics, please click on "Best answer" on the reply which solved your issue or answered your question.