2014-11-14 11:26 AM
In usb_regs.h wrong bits are assigned for register OTG_FS_DOEPCTL0 or OTG_HS_DOEPCTL0 to the structer typedef union _USB_OTG_DEPCTL_TypeDef.
Althought the names of bits are ok, their position doesn't match with with what the reference manual RM0090 Rev7 says about them. I am not sure if the lib actually uses this typedef but anyway. #usb #stm32 #library2014-11-17 03:02 AM
STM32F10x, STM32L1xx and STM32F3xx USB full speed device library
''. It doesn't support STM32F4 products.-Mayla-To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.