2020-08-28 4:23 AM
Hi. I'm tring to save data to usb memory stick. this is main fuction :
while (1)
{
/* USER CODE END WHILE */
MX_USB_HOST_Process();
/* USER CODE BEGIN 3 */
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
counter_start++;
if(f_mount(&myUsbFatFS, (TCHAR const*)USBH_Path, 0) == FR_OK)
{
UsbTest_Write();
}
break;
case APPLICATION_READY:
break;
case APPLICATION_DISCONNECT:
break;
}
}This is UsbTest_Write(); function
bool UsbTest_Write(void)
{
//Open or Create file for writing
if(f_open(&myFile, "a.csv", FA_WRITE | FA_OPEN_ALWAYS ) != FR_OK)
{
return 0;
}
//Copy test Text to my temporary read/write buffer
f_lseek(&myFile,myFile.fsize);
sprintf(rwtext, "asdfsdfsafdfadf\tasdfsdfsafdfadf\tasdfsdfsafdfadf\n");
//Write to text file
res = f_write(&myFile, (const void *)rwtext, strlen(rwtext), &byteswritten);
if((res != FR_OK) || (byteswritten == 0))
{
return 0;
f_close(&myFile);
}
f_close(&myFile);
return 1; //Success
}When ı connect usb stick it starts to write. After write 30-40 times it stop to writing. If i disconnect usb stick and connect again. It is write again 30-40 times. I looked in debug and put break point after
UsbTest_Write()
function this time it write just 1 time and
UsbTest_Write()
function always return 0 in this line
if(f_open(&myFile, "a.csv", FA_WRITE | FA_OPEN_ALWAYS ) != FR_OK)
{
return 0;
}
Why can be this happen and how can i solve?
2020-08-28 4:29 AM
Not going to be able to debug it at the top level.
Will need to instrument the DISKIO and USB-MSC level to understand the interactions. For bus level issues a USB Analyzer
2020-08-28 4:38 AM
I don't understand exactly how can i do this can you explain.
2020-08-30 11:10 PM
Hi @Community member I try to look deep and f_open->find_volume->check_fs->disk_read->USBH_MSC_Read
in usbh_msc.c USBH_MSC_Read function return USBH_FAIL with this
if ((phost->device.is_connected == 0U) ||
(phost->gState != HOST_CLASS) ||
(MSC_Handle->unit[lun].state != MSC_IDLE))
{
return USBH_FAIL;
}phost->device.is_connected = 0x01
phost->gState= HOST_ENMERATION
MSC_Handle->unit[lun].state = 0x7F
Do you have any suggestion ?