2025-02-06 7:23 AM
Hello,
I WOULD LIKE TO FIND AN EXAMPLE OF CODE FOR A USB HID CONNECTION WITH A STM32F429, A SIMPLE CODE (C#)
TO BE ABLE TO TURN ON AN LED IN MY SOFTWARE.
BY RECOVERING A CODE IN C# THAT WORKED WITH A MICROCHIP
TARGET AND BY CHANGING THE PID AND THE VID, CAN IT WORK WITH AN STM32?
Best regards
Sébastien
2025-02-06 11:27 AM - edited 2025-02-06 11:28 AM
Here is a very simple (if not primitive) example of driving a custom HID device from computer (Windows, Mac OS, Linux). Not C#, though you can port it to C# or make a "native" wrapper around the C++ library.
You can even make a simple firmware for your STM32 to simulate that HID device.