USB_Device/HID_Standalone Example project crashes on USB disconnect on B-L475E-IOT01A2
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-03-31 4:38 PM
Hi, I have a B-L475E-IOT01A2 board and I would like to implement an USB HID application on it. I use the example project found in the Github repository [1]. The application compiles and the USB device is detected on my computer as an input device. The problem is that upon a USB disconnect, the PC seems to jump to 0x0. When plugging the USB cable in again, the application runs again, but it seems I cannot run any code (in, e.g., the main while loop) after a USB disconnect interrupt while the cable is disconnected.
I see this problem both with STM32CubeIDE with ST-Link as well as with SEGGER j-link and Ozone.
In Ozone, I can set a breakpoint in the PCD Interrupt Handler for disconnect events (using USB_OTG_GINTSTS_OTGINT), which will trip upon disconnect. If I step through, I can finish HAL_PCD_IRQHandler to get back to OTG_FS_IRQHandler. As far as I can see, the PC clears to 0x0 after the POP {R7, PC} instruction which returns from the exception handler "OTG_FS_IRQHandler".
It can also be seen visually if I toggle an LED in the main while loop. After a USB disconnect, the blinking stops.
Steps to reproduce:
- Clone [1]
- Open STM32CubeIDE, go to File->Import
- Select 'Existing Projects into Workspace', Click Next and navigate to STM32CubeL4/Projects/B-L475E-IOT01A/Applications/USB_Device/HID_Standalone in the Git repo
- Debug the project, run it and plug in the USB OTG cable
- The device will enumerate as "STMicroelectronics HID Joystick in FS Mode" and your mouse will move
- Now disconnect the USB OTG cable and pause the execution
- Disassembly will fail as the PC is at 0x0
Any help regarding this issue would be greatly appreciated.
Thank you.
[1] https://github.com/STMicroelectronics/STM32CubeL4
Solved! Go to Solution.
- Labels:
-
USB
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-24 1:54 AM
Hello @exceptionthrower
The USB device is currently operating in low power mode, which limits its ability to perform debugging. To enable debugging, the low-power mode must be disabled. This can be achieved by adjusting the initialization settings in the `USBD_LL_Init()` function, available in the `usbd_conf.c` file.
Please refer to the code below for the exact changes that need to be made (line 13).
/**
* @brief Initializes the Low Level portion of the Device driver.
* @param pdev: Device handle
* @retval USBD Status
*/
USBD_StatusTypeDef USBD_LL_Init(USBD_HandleTypeDef *pdev)
{
/* Set LL Driver parameters */
hpcd.Instance = USB_OTG_FS;
hpcd.Init.dev_endpoints = 5;
hpcd.Init.use_dedicated_ep1 = 0;
hpcd.Init.dma_enable = 0;
hpcd.Init.low_power_enable = 0;
hpcd.Init.lpm_enable = 0;
hpcd.Init.battery_charging_enable = 0;
hpcd.Init.phy_itface = PCD_PHY_EMBEDDED;
hpcd.Init.Sof_enable = 0;
hpcd.Init.speed = PCD_SPEED_FULL;
hpcd.Init.vbus_sensing_enable = 1;
/* Link The driver to the stack */
hpcd.pData = pdev;
pdev->pData = &hpcd;
/* Initialize LL Driver */
HAL_PCD_Init(&hpcd);
/* configure EPs FIFOs */
HAL_PCDEx_SetRxFiFo(&hpcd, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd, 0, 0x40);
HAL_PCDEx_SetTxFiFo(&hpcd, 1, 0x80);
return USBD_OK;
}
Thanks
Omar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-09 3:02 AM
Hello @exceptionthrower
Thank you for bringing the issue to our attention. I have reported it internally.
Internal ticket number: 178547 (This is an internal tracking number and is not accessible or usable by customers).
Thanks
Omar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-17 1:14 AM
Hello @exceptionthrower
The issue you raised has been addressed and resolved internally. The fix will be integrated in an upcoming release. Thank you again for your contribution.
Thanks
Omar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-18 1:25 AM
Hello @exceptionthrower
To resolve the issue, you should remove the 100ms delay (line 6 in the code below) in the HAL_PCD_SuspendCallback
function located in the usbd_conf.c
file.
void HAL_PCD_SuspendCallback(PCD_HandleTypeDef *hpcd)
{
__HAL_PCD_GATE_PHYCLOCK(hpcd);
USBD_LL_Suspend(hpcd->pData);
HAL_Delay(100);
/*Enter in STOP mode */
if (hpcd->Init.low_power_enable)
{
/* Set SLEEPDEEP bit and SleepOnExit of Cortex System Control Register */
SCB->SCR |= (uint32_t)((uint32_t)(SCB_SCR_SLEEPDEEP_Msk | SCB_SCR_SLEEPONEXIT_Msk));
}
}
Thanks
Omar
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-18 3:05 AM
Hello @Saket_Om
Thank you for your reply.
I replicated the step above and removed the delay in the callback function (in a freshly cloned and compiled repository).
Unfortunately, the problem persists.
Thanks,
exceptionthrower
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2024-04-24 1:54 AM
Hello @exceptionthrower
The USB device is currently operating in low power mode, which limits its ability to perform debugging. To enable debugging, the low-power mode must be disabled. This can be achieved by adjusting the initialization settings in the `USBD_LL_Init()` function, available in the `usbd_conf.c` file.
Please refer to the code below for the exact changes that need to be made (line 13).
/**
* @brief Initializes the Low Level portion of the Device driver.
* @param pdev: Device handle
* @retval USBD Status
*/
USBD_StatusTypeDef USBD_LL_Init(USBD_HandleTypeDef *pdev)
{
/* Set LL Driver parameters */
hpcd.Instance = USB_OTG_FS;
hpcd.Init.dev_endpoints = 5;
hpcd.Init.use_dedicated_ep1 = 0;
hpcd.Init.dma_enable = 0;
hpcd.Init.low_power_enable = 0;
hpcd.Init.lpm_enable = 0;
hpcd.Init.battery_charging_enable = 0;
hpcd.Init.phy_itface = PCD_PHY_EMBEDDED;
hpcd.Init.Sof_enable = 0;
hpcd.Init.speed = PCD_SPEED_FULL;
hpcd.Init.vbus_sensing_enable = 1;
/* Link The driver to the stack */
hpcd.pData = pdev;
pdev->pData = &hpcd;
/* Initialize LL Driver */
HAL_PCD_Init(&hpcd);
/* configure EPs FIFOs */
HAL_PCDEx_SetRxFiFo(&hpcd, 0x80);
HAL_PCDEx_SetTxFiFo(&hpcd, 0, 0x40);
HAL_PCDEx_SetTxFiFo(&hpcd, 1, 0x80);
return USBD_OK;
}
Thanks
Omar