USB class implementation - MIDI interface
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-11-13 4:01 AM
Posted on November 13, 2013 at 13:01
Hello everybody !
I'm new here. I'm a musician, I code for 1 year on STM32 for the fun. My project is to create a MIDI controller based on STM32F4discovery (MIDI is a protocol created to allow musical instruments communication). I already program the code for the MIDI UART interface but the speed is quite limited and now I want to implement USB-MIDI, a popular protocol.So I want to send my MIDI packet (usually composed of 3 bytes) through the USB, and I also want my board to be recognized as a MIDI device. I have only one MIDI IN port IN and one MIDI port OUT.I try to understand on the internet how to achieve this but my problem is I don't know anything about USB librairies.Once I add the USB lib ''STM32_USB_Device_Library'' to my project, I don't find where I have to make changes in the source code (declaring 'input/output jacks', ''bulk endpoints'', ''protocol over endpoints'', ...) to implement the USB-MIDI.Do you know which files of the USB library I have to modify to create a recognized USB-MIDI peripherals ? Thanks for your help !!Some interresting stuff:/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Issues%20with%20STM32F4%20USB%20bulk%20transfer%20%28MIDI%29&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B¤tviews=942
#midi-usb
Labels:
- Labels:
-
Audio
This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Options
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2013-11-18 7:50 AM
Posted on November 18, 2013 at 16:50
Hello,
Maybe my question was not so easy or too specific... For the moment I add to my project ''usbd_audio_core.c'' and in this file there is a comment ://This driver doesn't implement the following aspects of the specification
//(but it is possible to manage these features with some modifications on this driver):
// - MIDI interfaces and modules
So it means that I need to add the Midi USB descriptor in this file. It looks like easy.
I know how to implement the MIDI descriptor thanks to an example ''Appendix B. Example: Simple MIDI Adapter (Informative)'' included in the
http://www.usb.org/developers/devclass_docs/midipdf
page So I need to create a new stucture likestatic
uint8_t usbd_audio_CfgDesc[AUDIO_CONFIG_DESC_SIZE] =
{
/* Configuration 1 */
0x09,
/* bLength */
USB_CONFIGURATION_DESCRIPTOR_TYPE,
/* bDescriptorType */
LOBYTE(AUDIO_CONFIG_DESC_SIZE),
/* wTotalLength 109 bytes*/
HIBYTE(AUDIO_CONFIG_DESC_SIZE),
0x02,
/* bNumInterfaces */
0x01,
/* bConfigurationValue */
0x00,
/* iConfiguration */
0xC0,
/* bmAttributes BUS Powred*/
0x32,
/* bMaxPower = 100 mA*/
/* 09 byte*/
but I need to replace theses informations by the description in the example included in the USB MIDI specification ? I'm really not sure of me...
Thanks !