cancel
Showing results for 
Search instead for 
Did you mean: 

when are the commands in the bootloader application notes used?

SBach.4
Associate II

In the Application Note for the ST Bootloader, DFU bootloader commands such as DFU_DNLOAD are specified. Where would I, as a programmer, use these commands? When communicating with the STM32 microcontroller using the ST Programmer via the command line, I have different commands. Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Pavel A.
Super User

Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

Of course it is.

View solution in original post

1 REPLY 1
Pavel A.
Super User

Does this mean the ST Programmer is an Application that uses that commands for its communication with the MC bootloader?

Of course it is.