cancel
Showing results for 
Search instead for 
Did you mean: 

Understanding bank swap when dual bank boot is enabled

guillaume petitjean
Associate II
Posted on May 15, 2018 at 14:21

Hello,

I'm developping a firmware on STM32L4x6.

I will use the dual bank boot mechanism for the firmware update feature. I've read AN2606 and AN4767 but I'm still confused about bank swap.

Does bank swap concern only code execution ? Or does it concern also any memory access from the MCU ? If the MCU reads some data from, for example, 0x08080000 ( first page of bank 2) while BFB2 is set, I understood the 'read memory' operation is 'translated' into a physical access to 0x08000000. Is it correct ?

What about the page erase sequence, where you have to specify the bank number and page number in FLASH_CR ?

What about the debugger output ? Is the memory also swapped for him ?

Best regards

#stm32-l4 #dual-bank-boot #flash-storage
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0