cancel
Showing results for 
Search instead for 
Did you mean: 

Unable to get DMA transfer complete to trigger

mleo2
Associate III

I'm using TIM1 to write a DMA buffer to the built-in LED. I'm trying to get the Transfer Complete callback to trigger. I've tried setting hdma->XferCpltCallback to a function. I suspect there is an interrupt enable flag I need to set and probably clear.

Here's my main.c:

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "dma.h" #include "tim.h" #include "usart.h" #include "gpio.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ #include <stdio.h> /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* USER CODE BEGIN PV */ // TIM_HandleTypeDef htim1; // DMA_HandleTypeDef hdma_tim1_up; // UART_HandleTypeDef huart2; /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); /* USER CODE BEGIN PFP */ // void SystemClock_Config(void); // void MX_GPIO_Init(void); // void MX_USART2_UART_Init(void); // void MX_DMA_Init(void); // void MX_TIM2_Init(void); #define PUTCHAR_PROTOTYPE int __io_putchar(int ch) /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ // void dmaComplete(DMA_HandleTypeDef *_hdma){ // UNUSED(_hdma); // printf("dma done\n"); // } void HAL_TIM_PWM_PulseFinishedCallback(TIM_HandleTypeDef *htim) { printf("DMA done\n"); } void HAL_TIM_PWM_PulseFinishedHalfCpltCallback(TIM_HandleTypeDef *htim) { printf("DMA half done\n"); } /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); MX_DMA_Init(); MX_TIM1_Init(); MX_USART2_UART_Init(); /* USER CODE BEGIN 2 */ uint32_t clockedData[13]; uint32_t count=0; for(int i=0;i<13;i++) clockedData[i]=0; // the clockedData goes straight to the BSRR register // [31 ... 16] are reset bits corresponding to Ports [15 ... 0] // [15 ... 0] are set bits corresponding to Ports [15 ... 0] // if a reset bit is set, the GPIO port will be set LOW // if a set bit is set, the GPIO port will be set HIGH clockedData[ 0] = 0x00000008; // LED on clockedData[ 1] = 0x00080000; // LED off clockedData[ 6] = 0x00000008; // LED on clockedData[12] = 0x00080000; // LED off // DMA, circular memory-to-peripheral mode, full word (32 bit) transfer HAL_DMA_Start(&hdma_tim1_up, (uint32_t)clockedData, (uint32_t)&(GPIOB->BSRR), 13); HAL_TIM_Base_Start(&htim1); HAL_TIM_OC_Start(&htim1, TIM_CHANNEL_1); TIM1->DIER |= (1 << 8); // set UDE bit (update dma request enable) // HAL_DMA_RegisterCallback(&hdma_tim1_up, HAL_DMA_XFER_CPLT_CB_ID,&dmaComplete); /* USER CODE END 2 */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ printf("\r\nTimer DMA Test %d", count); count++; // HAL_GPIO_TogglePin (GPIOB, GPIO_PIN_3); HAL_Delay(1000); /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Configure the main internal regulator output voltage */ if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK) { Error_Handler(); } /** Configure LSE Drive Capability */ HAL_PWR_EnableBkUpAccess(); __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_LOW); /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_LSE|RCC_OSCILLATORTYPE_MSI; RCC_OscInitStruct.LSEState = RCC_LSE_ON; RCC_OscInitStruct.MSIState = RCC_MSI_ON; RCC_OscInitStruct.MSICalibrationValue = 0; RCC_OscInitStruct.MSIClockRange = RCC_MSIRANGE_6; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON; RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_MSI; RCC_OscInitStruct.PLL.PLLM = 1; RCC_OscInitStruct.PLL.PLLN = 16; RCC_OscInitStruct.PLL.PLLP = RCC_PLLP_DIV7; RCC_OscInitStruct.PLL.PLLQ = RCC_PLLQ_DIV2; RCC_OscInitStruct.PLL.PLLR = RCC_PLLR_DIV2; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1|RCC_CLOCKTYPE_PCLK2; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_PLLCLK; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; RCC_ClkInitStruct.APB2CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_1) != HAL_OK) { Error_Handler(); } /** Enable MSI Auto calibration */ HAL_RCCEx_EnableMSIPLLMode(); } /* USER CODE BEGIN 4 */ /** * @brief Retargets the C library printf function to the USART. * None * @retval None */ PUTCHAR_PROTOTYPE { /* Place your implementation of fputc here */ /* e.g. write a character to the USART1 and Loop until the end of transmission */ HAL_UART_Transmit(&huart2, (uint8_t *)&ch, 1, 0xFFFF); return ch; } /* USER CODE END 4 */ /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

 

 

Here's tim.c where the DMA is setup and I assign the callback:

 

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file tim.c * @brief This file provides code for the configuration * of the TIM instances. ****************************************************************************** * @attention * * Copyright (c) 2024 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "tim.h" /* USER CODE BEGIN 0 */ #include <stdio.h> void dmaDone( DMA_HandleTypeDef * hdma){ printf("DMA DONE\r\n"); }; /* USER CODE END 0 */ TIM_HandleTypeDef htim1; DMA_HandleTypeDef hdma_tim1_up; /* TIM1 init function */ void MX_TIM1_Init(void) { /* USER CODE BEGIN TIM1_Init 0 */ /* USER CODE END TIM1_Init 0 */ TIM_ClockConfigTypeDef sClockSourceConfig = {0}; TIM_MasterConfigTypeDef sMasterConfig = {0}; /* USER CODE BEGIN TIM1_Init 1 */ /* USER CODE END TIM1_Init 1 */ htim1.Instance = TIM1; htim1.Init.Prescaler = 1000; htim1.Init.CounterMode = TIM_COUNTERMODE_UP; htim1.Init.Period = 4000; htim1.Init.ClockDivision = TIM_CLOCKDIVISION_DIV1; htim1.Init.RepetitionCounter = 0; htim1.Init.AutoReloadPreload = TIM_AUTORELOAD_PRELOAD_DISABLE; if (HAL_TIM_Base_Init(&htim1) != HAL_OK) { Error_Handler(); } sClockSourceConfig.ClockSource = TIM_CLOCKSOURCE_INTERNAL; if (HAL_TIM_ConfigClockSource(&htim1, &sClockSourceConfig) != HAL_OK) { Error_Handler(); } sMasterConfig.MasterOutputTrigger = TIM_TRGO_UPDATE; sMasterConfig.MasterOutputTrigger2 = TIM_TRGO2_RESET; sMasterConfig.MasterSlaveMode = TIM_MASTERSLAVEMODE_DISABLE; if (HAL_TIMEx_MasterConfigSynchronization(&htim1, &sMasterConfig) != HAL_OK) { Error_Handler(); } /* USER CODE BEGIN TIM1_Init 2 */ /* USER CODE END TIM1_Init 2 */ } void HAL_TIM_Base_MspInit(TIM_HandleTypeDef* tim_baseHandle) { if(tim_baseHandle->Instance==TIM1) { /* USER CODE BEGIN TIM1_MspInit 0 */ /* USER CODE END TIM1_MspInit 0 */ /* TIM1 clock enable */ __HAL_RCC_TIM1_CLK_ENABLE(); /* TIM1 DMA Init */ /* TIM1_UP Init */ hdma_tim1_up.Instance = DMA1_Channel6; hdma_tim1_up.Init.Request = DMA_REQUEST_7; hdma_tim1_up.Init.Direction = DMA_MEMORY_TO_PERIPH; hdma_tim1_up.Init.PeriphInc = DMA_PINC_DISABLE; hdma_tim1_up.Init.MemInc = DMA_MINC_ENABLE; hdma_tim1_up.Init.PeriphDataAlignment = DMA_PDATAALIGN_WORD; hdma_tim1_up.Init.MemDataAlignment = DMA_MDATAALIGN_WORD; hdma_tim1_up.Init.Mode = DMA_CIRCULAR;// DMA_NORMAL or DMA_CIRCULAR hdma_tim1_up.Init.Priority = DMA_PRIORITY_LOW; if (HAL_DMA_Init(&hdma_tim1_up) != HAL_OK) { Error_Handler(); } __HAL_LINKDMA(tim_baseHandle,hdma[TIM_DMA_ID_UPDATE],hdma_tim1_up); /* USER CODE BEGIN TIM1_MspInit 1 */ hdma_tim1_up.XferCpltCallback = &dmaDone; /* USER CODE END TIM1_MspInit 1 */ } } void HAL_TIM_Base_MspDeInit(TIM_HandleTypeDef* tim_baseHandle) { if(tim_baseHandle->Instance==TIM1) { /* USER CODE BEGIN TIM1_MspDeInit 0 */ /* USER CODE END TIM1_MspDeInit 0 */ /* Peripheral clock disable */ __HAL_RCC_TIM1_CLK_DISABLE(); /* TIM1 DMA DeInit */ HAL_DMA_DeInit(tim_baseHandle->hdma[TIM_DMA_ID_UPDATE]); /* USER CODE BEGIN TIM1_MspDeInit 1 */ /* USER CODE END TIM1_MspDeInit 1 */ } } /* USER CODE BEGIN 1 */ /* USER CODE END 1 */
View more

 

1 ACCEPTED SOLUTION

Accepted Solutions
mleo2
Associate III

I needed to use HAL_DMA_Start_IT(). This starts the DMA with interrupts enabled.

Is there someplace that has all this stuff documented? I found this by going through the source code.

View solution in original post

4 REPLIES 4
BarryWhit
Lead II

Did you remember to enable the DMA interrupt under the NVIC (Interrupt controller) peripheral in the CubeMX UI?

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.
mleo2
Associate III

I needed to use HAL_DMA_Start_IT(). This starts the DMA with interrupts enabled.

Is there someplace that has all this stuff documented? I found this by going through the source code.

mleo2
Associate III

Yes I did.

 

BarryWhit
Lead II

Is there someplace that has all this stuff documented? 

 

The HAL API follows a naming convention. Once you've used it for a while you know which function to call.

There's also a reference manual for the HAL for each family chip. For the G431 it's UM2570, for example.

 

- If someone's post helped resolve your issue, please thank them by clicking "Accept as Solution".
- Please post an update with details once you've solved your issue. Your experience may help others.