cancel
Showing results for 
Search instead for 
Did you mean: 

Touch Sensing channels count STM32L152ZE

patrick visser
Associate
Posted on April 12, 2018 at 12:30

Is there a error in theSTM32_TouchSensing_LibraryV2.1.1 with the maximum channel count for theSTM32L152ZE controller.

According to theUM1913 usermanual the STM32L1xx supports up to 34 channels.

STM32L1 series microcontrollers

– Surface charge-transfer acquisition principle managed by: – Two timers + routing interface (hardware acquisition mode). This mode is not supported on STM32L1 series microcontrollers featuring 256 K or less memory. – GPIOs + routing interface (software acquisition mode). This mode is supported by all microcontrollers. – Up to 34 channels – Up to 11 channels can be acquired simultaneously

But if you generate a new project with CubeMX the 'tsl_check_config_stm32l1xx.h' file has the following error checking functionality.

#if ((TSLPRM_TOTAL_CHANNELS < 1) || (TSLPRM_TOTAL_CHANNELS > 24))
#error 'TSLPRM_TOTAL_CHANNELS is out of range (1 .. 24).'
#endif
#if ((TSLPRM_TOTAL_BANKS < 1) || (TSLPRM_TOTAL_BANKS > 8))
#error 'TSLPRM_TOTAL_BANKS is out of range (1 .. 8).'
#endif
�?�?�?�?�?�?�?

these channel count does not comply with the uermanual or the datasheet of the controller.

How can I sample more then 24 channels?

I use Stm32CubeMX V4.0

STM32Cube FW_L1 V1.8.1

#cubemx-v4.0 #stm32l152
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0