2026-01-27 11:05 PM
Why is it that when I set the clock frequency of the STM32 to a high frequency (180 MHz), the code will crash, but when I set it to a low frequency (72 MHz), the code can run normally?
2026-01-28 12:17 AM - edited 2026-01-28 12:19 AM
Hello @乒乓 and welcome to the ST community,
What crystal value you've attached to HSE? you should not exceed 8MHz in that configuration.
2026-01-28 12:40 AM
The external clock I configured is 8 MHz.
2026-01-28 12:41 AM