cancel
Showing results for 
Search instead for 
Did you mean: 

STM32U5G9J- Dk board source code

PM.5
Associate III

Hi,

I recently purchased a STM32U5G9J -dk board. When I power up the board, TouchGFX demo application is running.

Can you please provide the source code of this demo application.

 

2 REPLIES 2
SirineST
ST Employee

Hello @PM.5 

I have reported this request internally. Internal ticket number: 189199 (This is an internal tracking number and is not accessible or usable by customers).

Thank you for your contribution

If your question is answered, please close this topic by clicking "Accept as Solution"
MOBEJ
ST Employee

Hello @PM.5 ,

In TouchGFX Designer, we offer an example that closely resembles the demo application on the STM32U5G9J-DK board. This demo is named "TouchGFX Demo 6" and can be found within the TouchGFX Designer. This tool is available as a standalone software application, making it easy and quick to evaluate graphics and develop proof-of-concept projects. It is included in the X-Cube-TouchGFX package, which you can download from the following link: TouchGFX Designer.

Br

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.