cancel
Showing results for 
Search instead for 
Did you mean: 

[stm32u585] wakeup failed from standby mode, "Wait till LSI is disabled" timeout in HAL_RCC_OscConfig()

lll
Associate III

hello,

I encountered a problem while developing for stm32u585. When the stm32 wakes up from standby mode, the HAL_RCC_OscConfig() function occasionally fails, "Wait till LSI is disabled" timeout in HAL_RCC_OscConfig() (this project uses IWDG)
The specific process is as follows:

1. start boot
    HAL_Init();
    SystemClock_Config();
    MX_GPIO_Init();
    MX_ICACHE_Init();
    MX_UART4_Init();
    boot to other address(app)
2. app init
    HAL_Init();
    SystemClock_Config();
          RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
                              |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
          RCC_OscInitStruct.HSEState = RCC_HSE_ON;
          RCC_OscInitStruct.LSEState = RCC_LSE_ON_RTC_ONLY;
          RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
          RCC_OscInitStruct.LSIState = RCC_LSI_ON;
          RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV128;
          RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
          RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
          RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
          RCC_OscInitStruct.PLL.PLLM = 1;
          RCC_OscInitStruct.PLL.PLLN = 40;
          RCC_OscInitStruct.PLL.PLLP = 2;
          RCC_OscInitStruct.PLL.PLLQ = 2;
          RCC_OscInitStruct.PLL.PLLR = 2;
          RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
          RCC_OscInitStruct.PLL.PLLFRACN = 0;
          if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
          {
            Error_Handler();
          }
3. timeout in HAL_RCC_OscConfig()
        /* Turn off LSI before changing RCC_BDCR_LSIPREDIV */
        if ((bdcr_temp & RCC_BDCR_LSION) == RCC_BDCR_LSION)
        {
          __HAL_RCC_LSI_DISABLE();

          tickstart = HAL_GetTick();

          /* Wait till LSI is disabled */
          while (READ_BIT(RCC->BDCR, RCC_BDCR_LSIRDY) != 0U)
          {
            if ((HAL_GetTick() - tickstart) > LSI_TIMEOUT_VALUE)
            {
              return HAL_TIMEOUT;
            }
          }
        }

How to solve this problem

 

1 ACCEPTED SOLUTION

Accepted Solutions
Saket_Om
ST Employee

Hello @lll 

The LSI should only be initialized once at power-on reset (POR). Re-initializing or reconfiguring the LSI after each wake-up from standby can cause issues, as the oscillator may already be in use by IWDG, and the LSIRDY flag may not behave as expected.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

View solution in original post

5 REPLIES 5
Saket_Om
ST Employee

Hello @lll 

The LSI should only be initialized once at power-on reset (POR). Re-initializing or reconfiguring the LSI after each wake-up from standby can cause issues, as the oscillator may already be in use by IWDG, and the LSIRDY flag may not behave as expected.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

Does this mean I have to modify HAL_RCC_OscConfig() ?

I have added this condition in HAL_RCC_OscConfig():

__HAL_PWR_GET_FLAG(PWR_FLAG_SBF)

Can it ensure that this startup is from standby wake-up

/*------------------------------ LSI Configuration -------------------------*/
  if ((((pRCC_OscInitStruct->OscillatorType) & RCC_OSCILLATORTYPE_LSI) == RCC_OSCILLATORTYPE_LSI)
      && __HAL_PWR_GET_FLAG(PWR_FLAG_SBF))

 

or modify SystemClock_Config()

  if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF))
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48
                                |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  else
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
                                |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;

 

Hello @lll 

In your own SystemClock_Config(), do not request LSI/LSIDiv changes when IWDG might already be running.
That way, HAL_RCC_OscConfig() never enters the “disable LSI” branch, so no timeout.

To give better visibility on the answered topics, please click on "Accept as Solution" on the reply which solved your issue or answered your question.
Saket_Om

Hello Saket_Om
In my SystemClock_Config():

void SystemClock_Config(void)
{
  RCC_OscInitTypeDef RCC_OscInitStruct = {0};
  RCC_ClkInitTypeDef RCC_ClkInitStruct = {0};

  /** Configure the main internal regulator output voltage
  */
  if (HAL_PWREx_ControlVoltageScaling(PWR_REGULATOR_VOLTAGE_SCALE1) != HAL_OK)
  {
    Error_Handler();
  }

  /** Configure LSE Drive Capability
  */
  HAL_PWR_EnableBkUpAccess();
  __HAL_RCC_LSEDRIVE_CONFIG(RCC_LSEDRIVE_MEDIUMHIGH);

  /** Initializes the CPU, AHB and APB buses clocks
  */
  if (__HAL_PWR_GET_FLAG(PWR_FLAG_SBF))
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48
                                |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  else
    RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI48|RCC_OSCILLATORTYPE_LSI
                                |RCC_OSCILLATORTYPE_HSE|RCC_OSCILLATORTYPE_LSE;
  RCC_OscInitStruct.HSEState = RCC_HSE_ON;
  RCC_OscInitStruct.LSEState = RCC_LSE_ON_RTC_ONLY;
  RCC_OscInitStruct.HSI48State = RCC_HSI48_ON;
  RCC_OscInitStruct.LSIState = RCC_LSI_ON;
  RCC_OscInitStruct.LSIDiv = RCC_LSI_DIV128;
  RCC_OscInitStruct.PLL.PLLState = RCC_PLL_ON;
  RCC_OscInitStruct.PLL.PLLSource = RCC_PLLSOURCE_HSE;
  RCC_OscInitStruct.PLL.PLLMBOOST = RCC_PLLMBOOST_DIV1;
  RCC_OscInitStruct.PLL.PLLM = 1;
  RCC_OscInitStruct.PLL.PLLN = 40;
  RCC_OscInitStruct.PLL.PLLP = 2;
  RCC_OscInitStruct.PLL.PLLQ = 2;
  RCC_OscInitStruct.PLL.PLLR = 2;
  RCC_OscInitStruct.PLL.PLLRGE = RCC_PLLVCIRANGE_1;
  RCC_OscInitStruct.PLL.PLLFRACN = 0;
  if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK)
  {
    Error_Handler();
  }

  ...
}

Is this correct? Now when waking up, it occasionally fails, sometimes even consecutively failing multiple times. Is there anything else that needs to be modified