2025-02-11 09:15 PM
Hi,
I am trying to use the AES hardware on the STM32U545 with the STM HAL libraries.
I am able to correctly encrypt and tag an number of bytes of plain text. However, whenever I try to decrypt an encrypted message with a length not divisible by 4 I get a tag mismatch but the decrypted plain text is correct.
I am using byte size data width for everything and have no header data.
From what I can see is that the encryption will work for any arbitrary size, however, the decryption tag is not computed correctly, unless the size is divisible by 4. Is this expected behavior or is this an issue with the HAL?
Thanks!
2025-02-12 01:39 AM
Hello @todor_digitalhealth ,
Hello as you can see in the readme file of STM32CubeU5/Projects/B-U585I-IOT02A/Examples/CRYP/CRYP_AES_GCM at main · STMicroelectronics/STM32CubeU5
"Plain text which will be authenticated and encrypted. Its size must be a multiple of 16 bytes. So if the original plain text size is not a multiple of 16 bytes, it must be padded."
also
So, you need to add extra padding to your plaintext if it is not multiple of 16 to get correct tags and this is normal behavior that you are seeing.
Regards
2025-02-12 08:02 PM
Thanks for the quick response S Tea!
I am able to successfully encrypt+tag and decrypt+verify tag if the plaintext message is 4, 8, or 12 bytes without having to pad the message. The HAL library can correctly encrypt and tag any size plaintext without any additional padding. The HAL decrypt function on the other hand can correctly decrypt the message (I get the correct plain text), however, the tag is not correct. I see that the function CRYP_AESGCM_Process in stm32u5xx_hal_cryp.c has code that handles the padding if the size is not a multiple of 16 bytes. Additionally, there is a case for setting the correct size for the tag calculation.
Thanks!