cancel
Showing results for 
Search instead for 
Did you mean: 

stm32u5 ux host hid with no vbus power

tommyliu
Associate

Hi,

I try to migrate the  UX_Host_HID example on STM32U575I-EV to nucleo-u575zi-q.

STM32CubeIDE Version: 1.17.0

STM32CubeMX Version: 6.13.0

I duplicate all the settings relating to USB host options to mine.

tommyliu_0-1737104641221.pngtommyliu_1-1737104671399.pngtommyliu_2-1737104689752.png

In the middleware:

tommyliu_3-1737104744759.pngtommyliu_4-1737104768241.png

tommyliu_5-1737104800940.pngtommyliu_6-1737104833337.png

and then copy the source code from the Ux_Host_HID

tommyliu_7-1737104935184.png

After programming the firmware to my ev board, i plug the hid device to the CN15 USB connector. There is noting happened and no power react on my hid device.

tommyliu_8-1737105169818.png

Did i miss any settings to setup the USB host example??

how can i provide power to the hid device???

 

Any response will be appreciated.

 

 

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
FBL
ST Employee

Hi @tommyliu 

It is an expected behavior. VBUS should be powered by the USB Host and the Nucleo-144 U575 board works as a USB Device. However, the eval board can work as usb host or device. Refer to section 7.13.1 Description in UM2854 and section 6.11 USB Type-C® FS/HS in UM2861 for more details.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.


View solution in original post

1 REPLY 1
FBL
ST Employee

Hi @tommyliu 

It is an expected behavior. VBUS should be powered by the USB Host and the Nucleo-144 U575 board works as a USB Device. However, the eval board can work as usb host or device. Refer to section 7.13.1 Description in UM2854 and section 6.11 USB Type-C® FS/HS in UM2861 for more details.

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.