Question
STM32L476 USB Termination
Posted on April 13, 2016 at 04:20
Hi folks,
I am a little confused about USB termination requirements on the STM32L476 part. I read in the datasheet that termination resistors on D+/D- are not needed and that the impedance matching is done by the internal PHY (as well as pull-up).However, I was reviewing the schematics for the STM32L4 Discovery board and it shows that termination resistors are used externally. As I would consider this a reference design, I am a bit confused by the discrepancy.Are the 22 Ohm termination resistors needed on D+/D- with this part or not?Thanks,RobPS -- This forum software is absolutely horrible. It is impossible to tell if this question has already been asked and answered. #usb #stm32l4-discovery-usb