cancel
Showing results for 
Search instead for 
Did you mean: 

STM32L475 IoT Node kit firmware update and fix for network credential entry?

TJM
Senior II

STM32L475 IoT Node has a firmware update with the STM32CubeExpansion_Cloud_AWS_V1.4.0 download. Firmware loads fine and the connection to a terminal for configuration takes place and shows the update version. The update will allow entry of the SSID and security mode but then 'Enter Password: ' prompt appears but does not allow the password entry but proceeds directly to the connection attempt, which fails without the password.

Is there an update or fix or a location in the code where I can fix this?

This discussion is locked. Please start a new topic to ask your question.
15 REPLIES 15
Vkamm.1
Associate III

Hi TJM,

Were you able to solve this problem? I am encountering the same problem.

Hi. I never did solve this issue. I admit that I'm still not comfortable or very knowledgeable with AWS and I suspect my problem was some issue with the AWS certificates​ or how they were being transmitted. I intend to get back to this in the near future but if you get it to work please post the resolution.

tjm​

Vkamm.1
Associate III

Hi TJM, I was able to solve the issue. I am able to connect and transfer data to AWS. I changed my policy setting attached to the thing. I allowed all incoming connections from AWS side. Do let me know if you were able to solve it?

HAarz.1
Associate II

Hi Vkamm.1,

I am stuck with the same issue. Can you tell a little bit more about how to allow incoming connections from AWS side ?

Thanks

Hi Vkamm.1,

I am stuck with the same issue. Can you tell a little bit more about how to allow incoming connections from AWS side ?

Thanks

Hi HAarz.1 ,

Can you ​check the attached policy to the thing on the AWS website. Does the policy allow all incoming connections? ​