Question
STM32L152 nucleo DFU mode example NOT RUN !!!!
The eaxample of dfu mode stm32l152 not run !!!
These are my step :
I build and execute code via IAR on Nucle0l152 board with usb _CN1 cable .
Then i dsconnected CN1 usb cable and i connected my USB cabel to PA11, PA12 , gnd and 5 v .
Then I open Open "DfuSe Demo" and download the "STM32L152xE_NUCLEO_SysTick_0x08007000.dfu" provided in Binary directory.
Then I upload the file.dfu .
Then i pressed reset on the board but led LD2 NOT BLINKING!!
WHY
Can help me .
Thanks .
Francy