STM32L151RET6 use low power run cause hardfault
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-06-18 6:41 PM - last edited on 2024-06-19 7:01 AM by Sarra.S
As title, MCU:STM32L151RET6, use freertos and enable tickless, when run PreSleepProcessing(uint32_t *ulExpectedIdleTime) function sometimes, cause hardfault. the sleep para is PWR_LOWPOWERREGULATOR_ON.
but when use PWR_MAINREGULATOR_ON, it's run OK.
The mcu sysclk is RCC_MSIRANGE_6, about 4MHz.
This phenomenon occurs only on a few boards.
Trace code discovery the last code run configPRE_SLEEP_PROCESSING( &xModifiableIdleTime ) in the function __weak void vPortSuppressTicksAndSleep( TickType_t xExpectedIdleTime ).
The performance is close to that of the substandard product?
__weak void PreSleepProcessing(uint32_t *ulExpectedIdleTime)
{
*ulExpectedIdleTime = 0;
// HAL_PWR_EnterSLEEPMode(PWR_MAINREGULATOR_ON, PWR_SLEEPENTRY_WFI);
HAL_PWR_EnterSLEEPMode(PWR_LOWPOWERREGULATOR_ON, PWR_SLEEPENTRY_WFI);
}
- Labels:
-
FreeRTOS
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2024-06-19 9:49 PM
In functiion HAL_PWR_EnterSLEEPMode(), I changed
if(SLEEPEntry == PWR_SLEEPENTRY_WFI)
{
/* Request Wait For Interrupt */
__WFI();
}
to
if(SLEEPEntry == PWR_SLEEPENTRY_WFI)
{
/* Request Wait For Interrupt */
__DSB();//add code
__WFI();
__NOP();//add code
__ISB();//add code
}
it worked normally.
if not change the code,and exchange two board's MCU, Every board works just fine. It looks like there's a difference in their performance.