STM32H743BIT ETHERNET UDP PACKET RECEIVING
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-05-22 10:25 PM
Hai ,
We are using the STM32H743BIT controller . we are using the cubemx to generate the code for the ethernet . In our application we need to receive the UDP packet which function we need to use . To send the UDP packet we are using the (UDP_packet_send(uint8_t *Tx_buf,uint16_t length)) function . Before this we are using the STM32F743BIT controller . But we took the the data from the (low_level_input(struct netif *netif)) from this function . Now we are not receiving any data .
Thank you.
best regards
Maheshwar.
#stm-32lo #udp #stm32h7-ethernet- Labels:
-
Ethernet
-
STM32L0 Series
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2018-06-27 6:35 AM
Hello
maheshwarreddy681
,Werecommend you to refer to the example provided in
/external-link.jspa?url=http%3A%2F%2Fwww.st.com%2Fen%2Fembedded-software%2Fstm32cubeh7.html
package andfollow the same configuration
:STM32Cube_FW_H7_V1.2.0\Projects\STM32H743ZI-Nucleo\Applications\LwIP\LwIP_HTTP_Server_Netconn_RTOS
With Regards,
Imen
Thanks
Imen