STM32H743 does not receive 29Bit-IDs on CAN
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-10-06 4:22 AM
Hello all,
I have an issue with receiving CAN Ids with 29 Bit IDs. 11 Bit IDs are working properly, but 29 Bit IDs are not received.
I do not use any filter setting, and in the GlobalFilter Setting I define to receive 29Bit IDs in FIFO0 or FIFO1 (desn't make a difference, Messages are not received with both settings).
Is there anything else which has to be activated to receive 29 Bit IDs?
Any ideas?
Here is my configuration:
...
halErr = HAL_FDCAN_Stop(phCan); // Stop CAN
if (sCanBusInit[nCan].bFDCAN != TRUE)
phCan->Init.FrameFormat = FDCAN_FRAME_CLASSIC;
else phCan->Init.FrameFormat = FDCAN_FRAME_FD_BRS;
if (sCanBusInit[nCan].nOperationMode != CAN_MODE_NORMAL)
{
phCan->Init.Mode = (uint32_t)sCanBusInit[nCan].nOperationMode; // Loop Intern/Extern or Listen only
}
else
{
phCan->Init.Mode = FDCAN_MODE_NORMAL;
CLEAR_BIT(phCan->Instance->CCCR, FDCAN_CCCR_TEST);
}
phCan->Init.AutoRetransmission = ENABLE;//Retransmission of disturbed Messages DISABLE;
phCan->Init.TransmitPause = DISABLE;
phCan->Init.NominalPrescaler = nNominalPrescaler;
phCan->Init.NominalSyncJumpWidth = 1;
phCan->Init.NominalTimeSeg1 = nNominalTimeSeg1;
phCan->Init.NominalTimeSeg2 = nNominalTimeSeg2;
phCan->Init.DataPrescaler = nDataPrescaler;
phCan->Init.DataSyncJumpWidth = 1;
phCan->Init.DataTimeSeg1 = nDataTimeSeg1;
phCan->Init.DataTimeSeg2 = nDataTimeSeg2;
phCan->Init.MessageRAMOffset = 0;
phCan->Init.StdFiltersNbr = 0;
phCan->Init.ExtFiltersNbr = 0;
phCan->Init.RxFifo0ElmtsNbr = 64; // 0..64
phCan->Init.RxFifo0ElmtSize = FDCAN_DATA_BYTES_8;
phCan->Init.RxFifo1ElmtsNbr = 64;
phCan->Init.RxFifo1ElmtSize = FDCAN_DATA_BYTES_8;
phCan->Init.RxBuffersNbr = 10;
phCan->Init.RxBufferSize = FDCAN_DATA_BYTES_8;
phCan->Init.TxEventsNbr = 0;
phCan->Init.TxBuffersNbr = 0;
phCan->Init.TxFifoQueueElmtsNbr = 1;
phCan->Init.TxFifoQueueMode = FDCAN_TX_FIFO_OPERATION;
phCan->Init.TxElmtSize = FDCAN_DATA_BYTES_8;
phCan->msgRam.StandardFilterSA = 0;
phCan->msgRam.ExtendedFilterSA = 0;
phCan->msgRam.RxFIFO0SA = 0;
phCan->msgRam.RxFIFO1SA = 0;
phCan->msgRam.RxBufferSA = 0;
phCan->msgRam.TxEventFIFOSA = 0;
phCan->msgRam.TxBufferSA = 0;
phCan->msgRam.TxFIFOQSA = 0;
phCan->msgRam.TTMemorySA = 0;
phCan->msgRam.EndAddress = 0;
phCan->ErrorCode = 0;
halErr = HAL_FDCAN_Init(phCan);
if (halErr != HAL_OK)
{
MyErrorHandler(E_CAN_DIV, halErr);
}
// Receive all IDs: 11-Bit in FIFO0, 29 Bit in FIFO1
HAL_FDCAN_ConfigGlobalFilter(phCan, FDCAN_ACCEPT_IN_RX_FIFO0, FDCAN_ACCEPT_IN_RX_FIFO1, FDCAN_REJECT, FDCAN_REJECT);
//FDCAN_REJECT_REMOTE, FDCAN_REJECT_REMOTE);
/* Start the FDCAN module */
halErr = HAL_FDCAN_Start(phCan);
halErr = HAL_FDCAN_ActivateNotification(phCan, FDCAN_IT_RX_FIFO0_NEW_MESSAGE, 0);
halErr = HAL_FDCAN_ActivateNotification(phCan, FDCAN_IT_RX_FIFO1_NEW_MESSAGE, 0);
- Labels:
-
CAN
-
STM32Cube MCU Packages
-
STM32H7 Series