cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H735G-DK HyperRAM Configuration Register Read failed

JKim.2
Senior

Hello,

I created the STM32H735G-DK project with the board selector in STM32CubeIDE.

The OSPI_HyperRAM_MemoryMapped project was created by the example selector. Its HyperRAM configuration register read codes were added to the STM32H735G-DK project as below. Writing data and reading data from the HyperRAM array work fine. However, both CR0 read and CR1 read returned INVALID_SEQUENCE error as below. Please help me to solve this problem.

Thanks.

 

S70KL1281_CR0_ADDRESS = 0x00001000
HAL_OSPI_HyperbusCmd: ErrorCode HAL_OSPI_ERROR_INVALID_SEQUENCE
Error from HAL_OSPI_HyperbusCmd

Read CR0 ERROR


S70KL1281_CR1_ADDRESS = 0x00001002
HAL_OSPI_HyperbusCmd: ErrorCode HAL_OSPI_ERROR_INVALID_SEQUENCE
Error from HAL_OSPI_HyperbusCmd

Read CR1 ERROR

 

  if (S70KL1281_ReadCfgReg0(&hospi2, &reg) != S70KL1281_OK) {
	  printf("\n\r");
	  printf("Read CR0 ERROR\n\r");
	  printf("\n\r");
  } else {
	  printf("Read CR0 = %08lx\n\r", reg);
  }
  if (S70KL1281_ReadCfgReg1(&hospi2, &reg) != S70KL1281_OK) {
	  printf("\n\r");
	  printf("Read CR1 ERROR\n\r");
	  printf("\n\r");
  } else {
	  printf("Read CR1 = %08lx\n\r", reg);
  }

 

 

 

int32_t S70KL1281_ReadCfgReg0(OSPI_HandleTypeDef *Ctx, uint16_t *Value)
{
  OSPI_HyperbusCmdTypeDef  sCommand;

  /* Initialize the read command */
  sCommand.AddressSpace = HAL_OSPI_REGISTER_ADDRESS_SPACE;
  sCommand.AddressSize  = HAL_OSPI_ADDRESS_32_BITS;
  sCommand.Address      = S70KL1281_CR0_ADDRESS;
  sCommand.DQSMode      = HAL_OSPI_DQS_ENABLE;
  sCommand.NbData       = 2U;								//number of bytes

  printf("\n\rS70KL1281_CR0_ADDRESS = 0x%08lx\n\r", S70KL1281_CR0_ADDRESS);
  /* Configure the command */
  if (HAL_OSPI_HyperbusCmd(Ctx, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
	printf("Error from HAL_OSPI_HyperbusCmd\n\r");
    return S70KL1281_ERROR;
  }

  /* Reception of the data */
  if (HAL_OSPI_Receive(Ctx, (uint8_t *)Value, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
	  printf("Error from HAL_OSPI_Receive\n\r");
    return S70KL1281_ERROR;
  }

  return S70KL1281_OK;
}

 

 

 

HAL_StatusTypeDef HAL_OSPI_HyperbusCmd(OSPI_HandleTypeDef *hospi, OSPI_HyperbusCmdTypeDef *cmd, uint32_t Timeout)
{
  HAL_StatusTypeDef status;
  uint32_t tickstart = HAL_GetTick();

  /* Check the parameters of the hyperbus command structure */
  assert_param(IS_OSPI_ADDRESS_SPACE(cmd->AddressSpace));
  assert_param(IS_OSPI_ADDRESS_SIZE (cmd->AddressSize));
  assert_param(IS_OSPI_NUMBER_DATA  (cmd->NbData));
  assert_param(IS_OSPI_DQS_MODE     (cmd->DQSMode));

  /* Check the state of the driver */
  if ((hospi->State == HAL_OSPI_STATE_READY) && (hospi->Init.MemoryType == HAL_OSPI_MEMTYPE_HYPERBUS))
  {
    /* Wait till busy flag is reset */
    status = OSPI_WaitFlagStateUntilTimeout(hospi, HAL_OSPI_FLAG_BUSY, RESET, tickstart, Timeout);

    if (status == HAL_OK)
    {
      /* Re-initialize the value of the functional mode */
      MODIFY_REG(hospi->Instance->CR, OCTOSPI_CR_FMODE, 0U);

      /* Configure the address space in the DCR1 register */
      MODIFY_REG(hospi->Instance->DCR1, OCTOSPI_DCR1_MTYP_0, cmd->AddressSpace);

      /* Configure the CCR and WCCR registers with the address size and the following configuration :
         - DQS signal enabled (used as RWDS)
         - DTR mode enabled on address and data
         - address and data on 8 lines */
      WRITE_REG(hospi->Instance->CCR, (cmd->DQSMode | OCTOSPI_CCR_DDTR | OCTOSPI_CCR_DMODE_2 |
                                       cmd->AddressSize | OCTOSPI_CCR_ADDTR | OCTOSPI_CCR_ADMODE_2));
      WRITE_REG(hospi->Instance->WCCR, (cmd->DQSMode | OCTOSPI_WCCR_DDTR | OCTOSPI_WCCR_DMODE_2 |
                                        cmd->AddressSize | OCTOSPI_WCCR_ADDTR | OCTOSPI_WCCR_ADMODE_2));

      /* Configure the DLR register with the number of data */
      WRITE_REG(hospi->Instance->DLR, (cmd->NbData - 1U));

      /* Configure the AR register with the address value */
      WRITE_REG(hospi->Instance->AR, cmd->Address);

      /* Update the state */
      hospi->State = HAL_OSPI_STATE_CMD_CFG;
    }
  }
  else
  {
    status = HAL_ERROR;
    hospi->ErrorCode = HAL_OSPI_ERROR_INVALID_SEQUENCE;
    printf("HAL_OSPI_HyperbusCmd: ErrorCode HAL_OSPI_ERROR_INVALID_SEQUENCE\n\r");
  }

  /* Return function status */
  return status;
}

 

 

 

static void MX_OCTOSPI2_Init(void)
{

  /* USER CODE BEGIN OCTOSPI2_Init 0 */

  /* USER CODE END OCTOSPI2_Init 0 */

  OSPIM_CfgTypeDef sOspiManagerCfg = {0};
  OSPI_HyperbusCfgTypeDef sHyperBusCfg = {0};

  /* USER CODE BEGIN OCTOSPI2_Init 1 */

  /* USER CODE END OCTOSPI2_Init 1 */
  /* OCTOSPI2 parameter configuration*/
  hospi2.Instance = OCTOSPI2;
  hospi2.Init.FifoThreshold = 4;
  hospi2.Init.DualQuad = HAL_OSPI_DUALQUAD_DISABLE;
  hospi2.Init.MemoryType = HAL_OSPI_MEMTYPE_HYPERBUS;
  hospi2.Init.DeviceSize = 32;
  hospi2.Init.ChipSelectHighTime = 8;
  hospi2.Init.FreeRunningClock = HAL_OSPI_FREERUNCLK_DISABLE;
  hospi2.Init.ClockMode = HAL_OSPI_CLOCK_MODE_0;
  hospi2.Init.WrapSize = HAL_OSPI_WRAP_NOT_SUPPORTED;
  hospi2.Init.ClockPrescaler = 4;
  hospi2.Init.SampleShifting = HAL_OSPI_SAMPLE_SHIFTING_NONE;
  hospi2.Init.DelayHoldQuarterCycle = HAL_OSPI_DHQC_ENABLE;		//HAL_OSPI_DHQC_DISABLE;
  hospi2.Init.ChipSelectBoundary = 23;
  hospi2.Init.DelayBlockBypass = HAL_OSPI_DELAY_BLOCK_USED;
  hospi2.Init.MaxTran = 0;
  hospi2.Init.Refresh = 250;
  if (HAL_OSPI_Init(&hospi2) != HAL_OK)
  {
    Error_Handler();
  }
  sOspiManagerCfg.ClkPort = 2;
  sOspiManagerCfg.DQSPort = 2;
  sOspiManagerCfg.NCSPort = 2;
  sOspiManagerCfg.IOLowPort = HAL_OSPIM_IOPORT_2_LOW;
  sOspiManagerCfg.IOHighPort = HAL_OSPIM_IOPORT_2_HIGH;
  if (HAL_OSPIM_Config(&hospi2, &sOspiManagerCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }
  sHyperBusCfg.RWRecoveryTime = 4;		//3.0V 100MHz tRWR spec 40nS
  sHyperBusCfg.AccessTime = 6;
  sHyperBusCfg.WriteZeroLatency = HAL_OSPI_LATENCY_ON_WRITE;	//HAL_OSPI_NO_LATENCY_ON_WRITE;
  sHyperBusCfg.LatencyMode = HAL_OSPI_FIXED_LATENCY;
  if (HAL_OSPI_HyperbusCfg(&hospi2, &sHyperBusCfg, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE BEGIN OCTOSPI2_Init 2 */
  /* Memory-mapped mode configuration --------------------------------------- */
  sCommand.AddressSpace = HAL_OSPI_MEMORY_ADDRESS_SPACE;
  sCommand.AddressSize  = HAL_OSPI_ADDRESS_32_BITS;
  sCommand.DQSMode      = HAL_OSPI_DQS_ENABLE;
  sCommand.Address      = 0;
  sCommand.NbData       = 1;

  if (HAL_OSPI_HyperbusCmd(&hospi2, &sCommand, HAL_OSPI_TIMEOUT_DEFAULT_VALUE) != HAL_OK)
  {
    Error_Handler();
  }

  sMemMappedCfg.TimeOutActivation = HAL_OSPI_TIMEOUT_COUNTER_DISABLE;

  if (HAL_OSPI_MemoryMapped(&hospi2, &sMemMappedCfg) != HAL_OK)
  {
    Error_Handler();
  }
  /* USER CODE END OCTOSPI2_Init 2 */

}

 

 

 

 

 

This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0