cancel
Showing results for 
Search instead for 
Did you mean: 

STM32H7 TFTP Server

jowakar122
Senior

I am trying to implement TFTP file transfer on my STM32 module (Nucleo-H723ZG). I have taken reference from:
https://github.com/STMicroelectronics/STM32CubeF4/tree/master/Projects/STM324xG_EVAL/Applications/LwIP/LwIP_IAP
https://github.com/JoeMerten/Stm32-Tools-Evaluation/tree/master/STM32Cube_FW_F4_V1.9.0/Projects/STM324xG_EVAL/Applications/LwIP/LwIP_TFTP_Server

For file transfer I am using tftpd64 software. I used the software for PC-PC file transfer which were on the same local network and it was successful. But when I am trying to send file from PC-STM32 module I am only receiving write request from the client (PC). After that  I am suppose the get a block 0 acknowledgement from the server (STM32 module) which I am not receiving. 

I tried debugging the code but in the code the acknowledgement is being sent successfully. For more information:
- my ethernet is up

- I have successfully ping the IP address that I have assigned or configured for the module.

- Moreover, I am using UDP so I am able to send messages using Hercules software.

Until the block 0 acknowledgement is received by the client (PC), it will not send the data packets.

20 REPLIES 20

I am using Nucleo-H723ZG which is not listed under the module which has LwIP_TFTP_Server.  The module I am using only has four example codes related to LwIP and none includes TFTP.

jowakar122_0-1743506949954.png

 

matt-crc
Senior III

lol.....

you said:

 

mattcrc_1-1743507288273.png

i gave you instructions how to download the project, you clearly didn't read it properly....

mattcrc_2-1743507409684.png

anyway... this is becoming a waste of my time.... lol

I used that for reference regarding ethernet and mpu configuration. In that example code SD card is used to store the file, whereas I am directly writing the file in the user flash memory which I will be receiving from the Ethernet.

jowakar122
Senior

jowakar122_2-1743508616653.png

My concern lies here. While debugging we can see that the local port, destination port, addr is correct and after executing the udp_sendto line I got err = 0 indicating that the acknowledgement so successfully sent. But it can be seen in wireshark nor the client proceeds to send the data packets.

 

Pavel A.
Super User

Have you checked for duplicate IP address? Someone else answers the ping?

I have cross checked about the duplicate IP address. When the ethernet is down ping on that same ip address has failed and it is not listed in arp. So there is not duplicate IP address.

jowakar122
Senior

Does anyone have any idea about this? It would be great.

jowakar122
Senior

For TFTP server to work properly it is recommended to use the tftp_server source and header files in Middleware. Earlier I was referring to the GitHub code in which a different file is created for initializing TFTP server, which came with many problems like mentioned above. After creating new project and by using this autogenerated files by STM32CubeIDE, I accomplished creating a TFTP server on stm module and transfer a file. 

Some points to consider when using this file:
- To initialize TFTP server we have to define the function pointers for handling file I/O operations. This structure is used by the TFTP server to manage file transfers, including opening, writing, and closing files. 

jowakar122_0-1744017902059.png

- This functions are called from the recv function in the tftp_server.c file.

jowakar122_1-1744018125776.png

 

Azelio
Associate II

Why the .read member of the struct is NULL?

@Azelio I have kept .read NULL because my stm32 module is working as TFTP server and in my case TFTP client was sending the file in 512 bytes of data packets. So only thing you are suppose to do is write the data packets in your flash, SD card etc. Moreover, there was no need for read function in my case.