STM32G071RB USBPD Sink with X-NUCLEO-USBPDM1 4 Errors after code-generation following example
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-08-12 11:16 AM
I have tried to follow this example:
Sadly right after code-generation there are already 4 errors without me adding the code as instructed in the document.
In usbpd_dpm_usr.c:
USBPD_StatusTypeDef USBPD_DPM_EvaluateDataRoleSwap(uint8_t PortNum)
{
/* USER CODE BEGIN USBPD_DPM_EvaluateDataRoleSwap */
USBPD_StatusTypeDef status = USBPD_REJECT;
if ((USBPD_TRUE == DPM_USER_Settings[PortNum].PE_DataSwap)
&& (((USBPD_TRUE == DPM_USER_Settings[PortNum].PE_DR_Swap_To_DFP) && (USBPD_PORTDATAROLE_UFP == DPM_Params[PortNum].PE_DataRole))
|| ((USBPD_TRUE == DPM_USER_Settings[PortNum].PE_DR_Swap_To_UFP) && (USBPD_PORTDATAROLE_DFP == DPM_Params[PortNum].PE_DataRole)))))
{
status = USBPD_ACCEPT;
}
return status;
/* USER CODE END USBPD_DPM_EvaluateDataRoleSwap */
}
results in 4 Errors. Specifically PE_DR_Swap_To_DFP and PE_DR_Swap_To_UFP do not seem to be named members of USBPD_USER_SettingsTypeDef.
After some searching I found that in gui_api.h really had no such members in USBPD_USER_SettingsTypeDef.
I am using the STM32CubeIDE Version 1.4.1, and have checked for all relevant updates I could find. In addition I tried using STM32CubeMX as shown in the document and the IAR IDE, which resulted in the same problem.
I would really appreciate getting some help from the community to get this example running.
Solved! Go to Solution.
- Labels:
-
STM32G0 Series
-
USB-PD
Accepted Solutions
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-02 6:49 AM
Hello
I imagine you enabled the GUI_INTERFACE feature. Unfortunately the structure 'USBPD_USER_SettingsTypeDef' in gui_api.h is not present in the current G0 FW package 1.3.0.
You can add manually the 2 parameters in the structure like this:
typedef struct
{
uint32_t PE_DataSwap : 1; /*!< support data swap */
uint32_t PE_VconnSwap : 1; /*!< support VCONN swap */
uint32_t PE_DR_Swap_To_DFP : 1U; /*!< If supported, DR Swap to DFP can be accepted or not by the user else directly rejected */
uint32_t PE_DR_Swap_To_UFP : 1U; /*!< If supported, DR Swap to UFP can be accepted or not by the user else directly rejected */
(...)
} USBPD_USER_SettingsTypeDef;
Regards,
Yohann
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
‎2020-09-02 6:49 AM
Hello
I imagine you enabled the GUI_INTERFACE feature. Unfortunately the structure 'USBPD_USER_SettingsTypeDef' in gui_api.h is not present in the current G0 FW package 1.3.0.
You can add manually the 2 parameters in the structure like this:
typedef struct
{
uint32_t PE_DataSwap : 1; /*!< support data swap */
uint32_t PE_VconnSwap : 1; /*!< support VCONN swap */
uint32_t PE_DR_Swap_To_DFP : 1U; /*!< If supported, DR Swap to DFP can be accepted or not by the user else directly rejected */
uint32_t PE_DR_Swap_To_UFP : 1U; /*!< If supported, DR Swap to UFP can be accepted or not by the user else directly rejected */
(...)
} USBPD_USER_SettingsTypeDef;
Regards,
Yohann