Skip to main content
SLin.6
Visitor II
May 3, 2023
Question

STM32G0 STM32MX generated PD source application generate hardreset every 14s

Hi, We have an PD source application on our custom board with STM32G071GBU6N. We use STM32 MX to genereate a PD source application (PD Core 4.1, device 3.4.1) following steps on

STM32StepByStep:Getting_started_with_USB-Power_Delivery_Source

After filling missing bits(Voltage monitoring and vbus switch and other DPM bits). we can make sink and source to enter a explicit power contract. but the PD stack will issue a PD hardreset every 14 seconds without any CAD events.

After few days of debugging, we finally resolve the issue by replacing PD stack library (USBPDCORE_PD3_FULL_CM0PLUS_wc32.a) from STM32 MX (4.1) with x-cube-tcpp_v4.0.0 (4.0) one.

Any sugguestions of starting our software project from STM32 generated one or from x-cube-tcpp_v4.0.0?

Regards

Steven

This topic has been closed for replies.

1 reply

HFISTM
ST Employee
May 22, 2023

Hello @SLin.6​ ,

A few questions:

Did you update some parts in Middlewares\ST\STM32_USBPD_Library\Devices\STM32G0XX component ?

Could you make sure that USBPD_HW_IF_GlobalHwInit() function is properly called during application start ?

Can you provide a dump of RCC->AHBENR register ?

That will help on debugging your issue.

Thanks & regards