cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F4DISCOVERY USB Audio Device works but ...

luhong
Associate
Posted on March 12, 2013 at 07:22

I have got the USB Audio Device example working on the stm32f4discovery board . When connected to my laptop via usb , the board can be recognized as an speaker. There is audio output from the headphone when play music on my laptop .However , the audio output is really funny , women sounds like man in the output of the board .

It seems that the I2S output clock frequency of the dicovery board is slightly higher than the audio sample rate of the laptop output . Is there a way to make the I2S output clock frequency the same with the audio sample rate of the laptop output?

-----------------------------------

I have changed the I2S input clock from 3840000 to 86000000 by generating another system_stm32f4xx.c file.It is much better now , still not perfect.

#stm32f4discovery-usb-audio
1 REPLY 1
Posted on March 05, 2014 at 09:23

I have the STMF4 Discovery working as USB Audio Sound Card.

Project and few details are here:

www.tjaekel.com

Best regards

Torsten