2012-12-25 8:46 PM
hi
how can I get high speed USB interface to host a device on STM32F4discovery? would i have to remove component from the kit OR just add additional PHY? #high-speed-usb #usb-otg #cpen #otg_hs #highspeed #metoo-not-quite #host_ctrl_xfer #vbus2013-01-14 1:30 AM
i have managed to run ULPI High speed interface with external EVAL board of USB3300 .
I am not able to modify the code available in audio record play back (for STM32f4discovery) to HIGH SPEED, I have made the important changes , but what i am missing here?. i have changed the OTG_FS to OTG_HS and define ULPI etc... I get to the point that Enumuraton is not done, I didnt get USBH_OK from function USBH_Handle_ENUM...(). and my Code get continuously pooling through HOST_CTRL_XFER after failed enumeration.2013-01-23 9:08 PM
i am using USB3300 SMSC eval board. I am able to run high speed ULPI interface with STM32F4 Discovery using MSC high speed example for STM324xx boards. I get a little highspeed than fullspeed. the ULPI is running well.
1=>I can write files to USB using ULPI highspeed interface, but I can't achieve High Data rate as expected. 2=> the speed get more lower about after 1000 files written, I am using character array of length 5 , name={'0','0','0','0','0'} and after when name={'0','1','0','0','0'} the speed get lower? why is that so? is due to the long file name I am using or what else? {if i refresh the name to 0,0,0,0,0 the speed get to its original} thanks2013-03-18 6:03 PM
Hey, i got question. How you managed to fix this problem when program was continuously pooling through HOST_CTRL_XFER after failed enumeration? I've got the same problem and i can't find solution.
2013-03-18 6:19 PM
Also I used MSC example for STM3210C-EVAL borad.
2013-03-19 6:51 AM
Also I used MSC example for STM3210C-EVAL borad.
So a bit off-topic then, perhaps a new thread with details of YOUR issue, and compiler settings, etc, might be a better route.2013-03-21 11:12 AM
Ok, I started new thread in
https://my.st.com/public/STe2ecommunities
>https://my.st.com/public/STe2ecommunities/mcu
> [DEAD LINK /public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?TopicsView=https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/AllItems.aspx¤tviews=0]STM32 >STM23F105RC USB OTG problem
link: https://my.st.com/public/STe2ecommunities/mcu/Lists/cortex_mx_stm32/Flat.aspx?RootFolder=%2fpublic%2fSTe2ecommunities%2fmcu%2fLists%2fcortex_mx_stm32%2fSTM23F105RC%20USB%20OTG%20problem&FolderCTID=0x01200200770978C69A1141439FE559EB459D7580009C4E14902C3CDE46A77F0FFD06506F5B&TopicsView=https%3A%2F%2Fm...2013-03-24 2:43 PM
Hey, tech.haris can you just tell me what did you do do deal with this continuous pooling through HOST_CTRL_XFER after failed enumeration? I know it might not relate at all to my problem, but since nobody want to say something I'll be very glad to get some hint.