2024-02-24 8:53 AM
Hi, i have build up a basic freertos and lwip setup. I just have one user task running.
I start a sntp to get the time and wanted to print the time in that task. But it does not reach there.
I get stuck. I'm using the cmsis v2 i recently upgraded the toolset of the IDE.
When i switch back to cmsis v1 it works. Any ideas?
Thanks
2024-02-24 12:53 PM
Ideas? Keep using CMSIS RTOS v1. It is not broken.
2024-02-24 1:18 PM
Hello @MOtto.2
Can you share your project here and indicate the modifications you've done between both working and not working projects.
Best Regards.
STTwo-32
To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.