cancel
Showing results for 
Search instead for 
Did you mean: 

stm32f439 freertos lwip stuck

MOtto.2
Associate II

Hi, i have build up a basic freertos and lwip setup. I just have one user task running. 

I start a sntp to get the time and wanted to print the time in that task. But it does not reach there.

I get stuck. I'm using the cmsis v2 i recently upgraded the toolset of the IDE.

When i switch back to cmsis v1 it works. Any ideas?

 

Thanks

2 REPLIES 2
Pavel A.
Evangelist III

Ideas? Keep using CMSIS RTOS v1. It is not broken.

 

STTwo-32
ST Employee

Hello @MOtto.2 

Can you share your project here and indicate the modifications you've done between both working and not working projects.

Best Regards.

STTwo-32 

To give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.