2020-03-27 7:19 AM
I have the STM32F429 Discovery development board. I want to send and receive data from the USB port. I will use Virtual Com Port for this. When I connect the Micro USB port on the card to the computer, it does not appear as a device. I use Keil as the compiler. My operating system is Windows 10.
Solved! Go to Solution.
2020-04-01 1:49 PM
You have installed a driver on your PC, but apparently there is no driver on the STM32F429.
Try compiling and installing an USB example from STM32CubeF4.
2020-03-27 7:23 AM
"data cable is not visible" ? You can't see the cable plugged into the board? I don't know how to parse this, seems like all is working correctly to me.
2020-03-27 7:29 AM
I installed the drivers that STM gave but it doesn't see micro usb connection in any way.
2020-03-27 9:31 AM
And what is that virtual COM Port thing in the device manager?
2020-03-27 10:07 AM
My problem is that it does not appear as a device when I connect micro usb. The programming cable of the com5 card shown in the picture, mini-b.
2020-03-27 11:07 PM
You need some software on the STM32F429 to configure the USB port as a serial communication device, and handle requests from the PC.
If there is no software to do that, the USB cable is just a piece of dangling wire as far as the PC can tell.
2020-04-01 11:31 AM
I installed the driver I mentioned above for this. But the computer does not see the card still connected. What should i do for the computer to see the micro usb connection ?? Is there anyone who can help ?
2020-04-01 1:49 PM
You have installed a driver on your PC, but apparently there is no driver on the STM32F429.
Try compiling and installing an USB example from STM32CubeF4.
2020-04-02 2:59 PM
Before seeing your suggestion, I solved my problem by using the example below. Thank you to Mr. Majerle and you.
https://stm32f4-discovery.net/2014/08/library-24-virtual-com-port-vcp-stm32f4xx/