2018-10-17 12:24 AM
When writing to RTC and then reading back, my year is always off - writing 18 gives me back 21. Tried adding delays up to a second between instructions, no joy. Using Cube and MDK, RTC is running LSE 32768 and works fine otherwise. Both read and write depend on HAL libraries that I haven't touched.
typedef struct __TIME_INFO
{
RTC_TimeTypeDef sTime;
RTC_DateTypeDef sDate;
} TIME_INFO;
void rtc_updateRTCclock(TIME_INFO *t)
{
HAL_RTC_SetTime(&MAIN_RTC, &(t->sTime), RTC_FORMAT_BIN);
HAL_RTC_SetDate(&MAIN_RTC, &(t->sDate), RTC_FORMAT_BIN);
}
TIME_INFO rtc_getCurrentTime() {
TIME_INFO t;
HAL_RTC_GetTime(&MAIN_RTC, &(t.sTime), RTC_FORMAT_BIN);
HAL_RTC_GetDate(&MAIN_RTC, &(t.sDate), RTC_FORMAT_BIN);
return t;
}
2019-01-17 6:28 AM
I had the same problem. I found that the problem was not setting the WeekDay (when creating a struct RTC_DateTypeDef, the field WeekDay gets a random value). The value WeekDay must be set to a value between 0 to 7.
Explanation: The code for setting the date in function HAL_RTC_SetDate:
if (Format == RTC_FORMAT_BIN)
{
assert_param(IS_RTC_YEAR(sDate->Year));
assert_param(IS_RTC_MONTH(sDate->Month));
assert_param(IS_RTC_DATE(sDate->Date));
datetmpreg = (((uint32_t)RTC_ByteToBcd2(sDate->Year) << 16U) | \
((uint32_t)RTC_ByteToBcd2(sDate->Month) << 8U) | \
((uint32_t)RTC_ByteToBcd2(sDate->Date)) | \
((uint32_t)sDate->WeekDay << 13U));
}
else
{
assert_param(IS_RTC_YEAR(RTC_Bcd2ToByte(sDate->Year)));
assert_param(IS_RTC_MONTH(RTC_Bcd2ToByte(sDate->Month)));
assert_param(IS_RTC_DATE(RTC_Bcd2ToByte(sDate->Date)));
datetmpreg = ((((uint32_t)sDate->Year) << 16U) | \
(((uint32_t)sDate->Month) << 8U) | \
((uint32_t)sDate->Date) | \
(((uint32_t)sDate->WeekDay) << 13U));
}When WeekDay is greater than 7, it overlaps with the bits of Year and can change it.
2019-01-17 6:55 AM
> When WeekDay is greater than 7, it overlaps with the bits of Year and can change it
So you've found a bug in the HAL library where the function does not validate sDate->WeekDay input value.
-- pa
2019-01-17 3:01 PM
> So you've found a bug in the HAL library where the function does not validate sDate->WeekDay input value.
There's no bug. There is an assertion just above those lines - see my previous post.
JW