2014-10-23 07:37 AM
Hello All,
We are using STM32F407VG & are having issues with bootloader via USART3 PC10/PC11. From the SW, we see that the processor is entering the bootloader mode.When 0x7F is send, the processor responds with ''0x00 0x00 0x00'' instead of 0x79.We are using BR-9600, 8Bit, Even parity & 1 stop bit. We have been struggling for over a week now & have no clue what we are missing. Looking for some help or guidance!Thanks in advance. #discovery #stm32 #stm32f4 #bootloader2014-10-23 07:49 AM
How and to what are you connecting it? The STM32 uses CMOS Serial levels, these are not compatible with RS232 signalling levels.
2014-10-23 02:33 PM
Hi Clive1,
Thanks for your reply.We are connected to a PC (Widnows 😎 comp port. On the STM32F4 side we are using TRS3223E. I have attached the circuit diagram as well for reference.