STM32F105 unable to detect USB memory stick removal
- Mark as New
- Bookmark
- Subscribe
- Mute
- Subscribe to RSS Feed
- Permalink
- Email to a Friend
- Report Inappropriate Content
2019-05-08 6:56 PM
Hello All, I m using STM32F105R8 as USB Host to read and write files to USB memory stick with HAL lib. Cube FW version STM32Cube_FW_F1_V1.7.0.
Setup:
1) Custom board with STM32F105R8 as USB host and USB socket for inserting USB memory stick (pen drive). It is basically a Datalogger project to store data in USB pen drive
2) USB Memory stick is powered by the uC board with its own 5v. Vbus sensing is used but i assume it is of no use the board is powering up all the time
3) I have not pulled up or pulled down the DP and DM lines of USB. ESD protection circuit is implemented with USBUF01W6. I assume as a HOST board, I dont need to pull up of DP with 1.5k.
Problem:
1) If I power up the board with USB already inserted, then MX_USB_HOST_Process() is able to start, enumerate and come to ready state. I could read write files using FATFS - This has no problem
2) The issue is : After power on, If I simply disconnect the USB memory stick, then no change in the Appli_state. I does not go to disconnect state at all. It is not able to recognize the disconnect.
3) If I insert the Memory stick again, it could not detect the new device anymore. Further file operation hangs the uC
4) As I mentioned in #1, If the USB is inserted since power on, it works fine and during file operation If i disconnect, then after several seconds it recovers after that it is not able to detect if I insert the memory stick again.
Question:
How to make the uC to detect the USB mass storage device is inserted as well able to detect the removal.
I call this in while under main()
void USB_HOST_BACKGROUND_TASK(void)
{
MX_USB_HOST_Process();
switch(Appli_state)
{
case APPLICATION_IDLE:
break;
case APPLICATION_START:
if(f_mount(&myUSBfatfs,(TCHAR const*)USBHPath,0) != FR_OK)
{
Error_Handler();
}
else
{
}
break;
case APPLICATION_READY:
ResetMicros();
if(tmst>10)
{
if(!B_f)
{
B_f=1;
//UsbTest_Write();
f_open(&myFile1, "file1.TXT", FA_WRITE | FA_CREATE_ALWAYS);
f_open(&myFile2, "file2.TXT", FA_WRITE | FA_CREATE_ALWAYS);
}
else if(tmst<20)
{
sprintf(rwtext, "\r\nHello from Balaji Ramalingam %ul",timer1ms_l);
//Write to text file
f_write(&myFile1, (const void *)rwtext, strlen(rwtext), &byteswritten);
sprintf(rwtext, "\r\nHello from Balaji Ramalingam %ul",timer1ms_l+100);
f_write(&myFile2, (const void *)rwtext, strlen(rwtext), &byteswritten);
}
else if(tmst==21)
{
f_close(&myFile1);
f_close(&myFile2);
}
}
GetMicros();
break;
case APPLICATION_DISCONNECT:
//output_write(0,op_PWMLED2)
break;
}
}
- Labels:
-
STM32Cube MCU Packages
-
STM32F1 Series
-
USB