cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 STM32CubeMX USB CDC problem

erdem
Associate
Posted on December 16, 2014 at 09:29

Hi guys 

I have a project with STM32F042K6 . My design will get datas via USB  CDC (communication device class ) from PC and it stores datas to a FLASH memory. After a while it will send datas to another device via UART. 

1-). STM32CubeMx  can not generate a compilable code for STM32F042K6 because of  

MAX_STATIC_ALLOC_SIZE.

I change it 140 and now it can be compile.

2-) My test program work like this ; I send datas (''STM32'') to PC via USB continously . I  send datas (1 byte or 2 byte or 3 byte..) to my board via USB from PC and no problem. but when I send 7 byte data ( string data like ''STM32F0'') to my board , the data (''STM32'') that I send to PC automaticly changes. My program start to send meaningless data to PC .  

Can any body help me ? You can find my project files in below link.

http://www.filedropper.com/den4

#stm32f0 #cdc #usb
This discussion is locked. Please start a new topic to ask your question.
0 REPLIES 0