STM32 MCUs Embedded software

Ask questions and find answers on STM32Cube packages, including HAL, LL and middleware, and expansion software.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Bug in LL library for stm32f1xx

Posted on September 27, 2017 at 19:03I want to turn on the led attached to PC.9. I do this:    LL_GPIO_InitTypeDef initStruct;    LL_GPIO_StructInit( &initStruct );        initStruct.Mode = LL_GPIO_MODE_OUTPUT_10MHz;    initStruct.OutputType = LL_GP...

amomum by Associate III
  • 9296 Views
  • 20 replies
  • 1 kudos

STM32F410 Reference manual incomplete

Posted on March 09, 2018 at 12:36Hello ST,I found that STM32F410 reference manual is incomplete:http://www.st.com/resource/en/reference_manual/dm00180366.pdf There are no bootloader interfaces for UFBGA64 and LQFP48 packages in the table 3 on page 4...

0690X0000060A2aQAE.png
Eugene S. by Associate III
  • 2227 Views
  • 4 replies
  • 0 kudos

WRP bits not working ?

Posted on March 22, 2018 at 11:06Hi,I am working with the STM32f407 : I have a bootloader in the first flash sector (ie. @ 0x0800 0000), and my main program in the following sectors (ie. @ 0x0800 4000). I want to protect my bootloader against unwant...

STM32F3: USB Vendor Class?

Posted on June 14, 2017 at 12:20Hi,I'm using STM32F303VB in my custom hardware that has USB.When using STM32CubeMX I see a lot of Standard USB Device classes that I can use (Audio Class, HID, Custom HID,.. etc..). But I do not see an option for Vend...

Prasant J by Associate III
  • 1406 Views
  • 1 replies
  • 1 kudos

FreeRTOS+FatFs+SD+DMA

Posted on March 23, 2018 at 03:40Still having issues with tracking down how this is supposed to work using F746G-Discovery board, F7V1.11.0 CubeMX, with the board configured to use FreeRTOS, FatFs, SDMMC, and DMA.  Everything is fine up to f_close, ...

QSPI + FatFS + USB mass storage

Posted on March 21, 2018 at 15:12 Hello there, I am trying to connect 3 sub-systems: qspi flash memoryFatFSUSB mass storage device I have successfully written low level drivers for qspi and have connected it with FatFS middleware. I can read ...

STM32F405RG USB FS (device mode) not working

Posted on March 23, 2018 at 18:36Dear all,I am having some issues making the USB FS to work using the STM32F405 microcontroller. The setup is pretty simple by following the guidelines found in this forum, however it still not working. My custom boar...

Io D by Associate II
  • 753 Views
  • 0 replies
  • 0 kudos