cancel
Showing results for 
Search instead for 
Did you mean: 

STM32F0 minimal RTOS example doesn't work

vas
Associate II

Hi fellow engineers,

I'm trying to create a minimal example of blinky using an RTOS task in STM32CubeIDE. My MCU is a bare STM32F070CBT6. The code ends up in Default_Handler just a moment after the start

WWDG_IRQHandler stop.png

IOC file is as follows, nothing is configured, except FREERTOS, GPIO port for the LED and TIM6 as timebase source

#MicroXplorer Configuration settings - do not modify CAD.formats= CAD.pinconfig= CAD.provider= FREERTOS.IPParameters=Tasks01 FREERTOS.Tasks01=defaultTask,24,128,StartDefaultTask,Default,NULL,Dynamic,NULL,NULL File.Version=6 GPIO.groupedBy=Group By Peripherals KeepUserPlacement=false Mcu.CPN=STM32F070CBT6 Mcu.Family=STM32F0 Mcu.IP0=FREERTOS Mcu.IP1=NVIC Mcu.IP2=RCC Mcu.IP3=SYS Mcu.IPNb=4 Mcu.Name=STM32F070CBTx Mcu.Package=LQFP48 Mcu.Pin0=PC13 Mcu.Pin1=VP_FREERTOS_VS_CMSIS_V2 Mcu.Pin2=VP_SYS_VS_tim6 Mcu.PinsNb=3 Mcu.ThirdPartyNb=0 Mcu.UserConstants= Mcu.UserName=STM32F070CBTx MxCube.Version=6.13.0 MxDb.Version=DB.6.0.130 NVIC.ForceEnableDMAVector=true NVIC.HardFault_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.NonMaskableInt_IRQn=true\:0\:0\:false\:false\:true\:false\:false\:false\:false NVIC.PendSV_IRQn=true\:3\:0\:false\:false\:false\:true\:false\:false\:false NVIC.SVC_IRQn=true\:0\:0\:false\:false\:false\:false\:false\:false\:true NVIC.SavedPendsvIrqHandlerGenerated=true NVIC.SavedSvcallIrqHandlerGenerated=true NVIC.SavedSystickIrqHandlerGenerated=true NVIC.SysTick_IRQn=true\:3\:0\:false\:false\:false\:true\:false\:true\:false NVIC.TIM6_IRQn=true\:3\:0\:false\:false\:true\:false\:false\:true\:true NVIC.TimeBase=TIM6_IRQn NVIC.TimeBaseIP=TIM6 PC13.GPIOParameters=GPIO_Label PC13.GPIO_Label=LED_G PC13.Locked=true PC13.Signal=GPIO_Output PinOutPanel.RotationAngle=0 ProjectManager.AskForMigrate=true ProjectManager.BackupPrevious=false ProjectManager.CompilerOptimize=6 ProjectManager.ComputerToolchain=false ProjectManager.CoupleFile=false ProjectManager.CustomerFirmwarePackage= ProjectManager.DefaultFWLocation=true ProjectManager.DeletePrevious=true ProjectManager.DeviceId=STM32F070CBTx ProjectManager.FirmwarePackage=STM32Cube FW_F0 V1.11.5 ProjectManager.FreePins=false ProjectManager.HalAssertFull=false ProjectManager.HeapSize=0x200 ProjectManager.KeepUserCode=true ProjectManager.LastFirmware=true ProjectManager.LibraryCopy=1 ProjectManager.MainLocation=Core/Src ProjectManager.NoMain=false ProjectManager.PreviousToolchain= ProjectManager.ProjectBuild=false ProjectManager.ProjectFileName=FreeRTOS_ThreadCreation.ioc ProjectManager.ProjectName=FreeRTOS_ThreadCreation ProjectManager.ProjectStructure= ProjectManager.RegisterCallBack= ProjectManager.StackSize=0x400 ProjectManager.TargetToolchain=STM32CubeIDE ProjectManager.ToolChainLocation= ProjectManager.UAScriptAfterPath= ProjectManager.UAScriptBeforePath= ProjectManager.UnderRoot=true ProjectManager.functionlistsort=1-SystemClock_Config-RCC-false-HAL-false RCC.FamilyName=M RCC.IPParameters=FamilyName,PLLCLKFreq_Value,PLLMCOFreq_Value,TimSysFreq_Value,USBOutputFreqValue,VCOOutput2Freq_Value RCC.PLLCLKFreq_Value=16000000 RCC.PLLMCOFreq_Value=16000000 RCC.TimSysFreq_Value=8000000 RCC.USBOutputFreqValue=16000000 RCC.VCOOutput2Freq_Value=8000000 VP_FREERTOS_VS_CMSIS_V2.Mode=CMSIS_V2 VP_FREERTOS_VS_CMSIS_V2.Signal=FREERTOS_VS_CMSIS_V2 VP_SYS_VS_tim6.Mode=TIM6 VP_SYS_VS_tim6.Signal=SYS_VS_tim6 board=custom isbadioc=false
View more

The only change in the main.c is the LED toggle

/* USER CODE BEGIN Header */ /** ****************************************************************************** * @file : main.c * @brief : Main program body ****************************************************************************** * @attention * * Copyright (c) 2025 STMicroelectronics. * All rights reserved. * * This software is licensed under terms that can be found in the LICENSE file * in the root directory of this software component. * If no LICENSE file comes with this software, it is provided AS-IS. * ****************************************************************************** */ /* USER CODE END Header */ /* Includes ------------------------------------------------------------------*/ #include "main.h" #include "cmsis_os.h" /* Private includes ----------------------------------------------------------*/ /* USER CODE BEGIN Includes */ /* USER CODE END Includes */ /* Private typedef -----------------------------------------------------------*/ /* USER CODE BEGIN PTD */ /* USER CODE END PTD */ /* Private define ------------------------------------------------------------*/ /* USER CODE BEGIN PD */ /* USER CODE END PD */ /* Private macro -------------------------------------------------------------*/ /* USER CODE BEGIN PM */ /* USER CODE END PM */ /* Private variables ---------------------------------------------------------*/ /* Definitions for defaultTask */ osThreadId_t defaultTaskHandle; const osThreadAttr_t defaultTask_attributes = { .name = "defaultTask", .stack_size = 128 * 4, .priority = (osPriority_t) osPriorityNormal, }; /* USER CODE BEGIN PV */ /* USER CODE END PV */ /* Private function prototypes -----------------------------------------------*/ void SystemClock_Config(void); static void MX_GPIO_Init(void); void StartDefaultTask(void *argument); /* USER CODE BEGIN PFP */ /* USER CODE END PFP */ /* Private user code ---------------------------------------------------------*/ /* USER CODE BEGIN 0 */ /* USER CODE END 0 */ /** * @brief The application entry point. * @retval int */ int main(void) { /* USER CODE BEGIN 1 */ /* USER CODE END 1 */ /* MCU Configuration--------------------------------------------------------*/ /* Reset of all peripherals, Initializes the Flash interface and the Systick. */ HAL_Init(); /* USER CODE BEGIN Init */ /* USER CODE END Init */ /* Configure the system clock */ SystemClock_Config(); /* USER CODE BEGIN SysInit */ /* USER CODE END SysInit */ /* Initialize all configured peripherals */ MX_GPIO_Init(); /* USER CODE BEGIN 2 */ /* USER CODE END 2 */ /* Init scheduler */ osKernelInitialize(); /* USER CODE BEGIN RTOS_MUTEX */ /* add mutexes, ... */ /* USER CODE END RTOS_MUTEX */ /* USER CODE BEGIN RTOS_SEMAPHORES */ /* add semaphores, ... */ /* USER CODE END RTOS_SEMAPHORES */ /* USER CODE BEGIN RTOS_TIMERS */ /* start timers, add new ones, ... */ /* USER CODE END RTOS_TIMERS */ /* USER CODE BEGIN RTOS_QUEUES */ /* add queues, ... */ /* USER CODE END RTOS_QUEUES */ /* Create the thread(s) */ /* creation of defaultTask */ defaultTaskHandle = osThreadNew(StartDefaultTask, NULL, &defaultTask_attributes); /* USER CODE BEGIN RTOS_THREADS */ /* add threads, ... */ /* USER CODE END RTOS_THREADS */ /* USER CODE BEGIN RTOS_EVENTS */ /* add events, ... */ /* USER CODE END RTOS_EVENTS */ /* Start scheduler */ osKernelStart(); /* We should never get here as control is now taken by the scheduler */ /* Infinite loop */ /* USER CODE BEGIN WHILE */ while (1) { /* USER CODE END WHILE */ /* USER CODE BEGIN 3 */ } /* USER CODE END 3 */ } /** * @brief System Clock Configuration * @retval None */ void SystemClock_Config(void) { RCC_OscInitTypeDef RCC_OscInitStruct = {0}; RCC_ClkInitTypeDef RCC_ClkInitStruct = {0}; /** Initializes the RCC Oscillators according to the specified parameters * in the RCC_OscInitTypeDef structure. */ RCC_OscInitStruct.OscillatorType = RCC_OSCILLATORTYPE_HSI; RCC_OscInitStruct.HSIState = RCC_HSI_ON; RCC_OscInitStruct.HSICalibrationValue = RCC_HSICALIBRATION_DEFAULT; RCC_OscInitStruct.PLL.PLLState = RCC_PLL_NONE; if (HAL_RCC_OscConfig(&RCC_OscInitStruct) != HAL_OK) { Error_Handler(); } /** Initializes the CPU, AHB and APB buses clocks */ RCC_ClkInitStruct.ClockType = RCC_CLOCKTYPE_HCLK|RCC_CLOCKTYPE_SYSCLK |RCC_CLOCKTYPE_PCLK1; RCC_ClkInitStruct.SYSCLKSource = RCC_SYSCLKSOURCE_HSI; RCC_ClkInitStruct.AHBCLKDivider = RCC_SYSCLK_DIV1; RCC_ClkInitStruct.APB1CLKDivider = RCC_HCLK_DIV1; if (HAL_RCC_ClockConfig(&RCC_ClkInitStruct, FLASH_LATENCY_0) != HAL_OK) { Error_Handler(); } } /** * @brief GPIO Initialization Function * @PAram None * @retval None */ static void MX_GPIO_Init(void) { GPIO_InitTypeDef GPIO_InitStruct = {0}; /* USER CODE BEGIN MX_GPIO_Init_1 */ /* USER CODE END MX_GPIO_Init_1 */ /* GPIO Ports Clock Enable */ __HAL_RCC_GPIOC_CLK_ENABLE(); /*Configure GPIO pin Output Level */ HAL_GPIO_WritePin(LED_G_GPIO_Port, LED_G_Pin, GPIO_PIN_RESET); /*Configure GPIO pin : LED_G_Pin */ GPIO_InitStruct.Pin = LED_G_Pin; GPIO_InitStruct.Mode = GPIO_MODE_OUTPUT_PP; GPIO_InitStruct.Pull = GPIO_NOPULL; GPIO_InitStruct.Speed = GPIO_SPEED_FREQ_LOW; HAL_GPIO_Init(LED_G_GPIO_Port, &GPIO_InitStruct); /* USER CODE BEGIN MX_GPIO_Init_2 */ /* USER CODE END MX_GPIO_Init_2 */ } /* USER CODE BEGIN 4 */ /* USER CODE END 4 */ /* USER CODE BEGIN Header_StartDefaultTask */ /** * @brief Function implementing the defaultTask thread. * @PAram argument: Not used * @retval None */ /* USER CODE END Header_StartDefaultTask */ void StartDefaultTask(void *argument) { /* USER CODE BEGIN 5 */ /* Infinite loop */ for(;;) { HAL_GPIO_TogglePin(LED_G_GPIO_Port, LED_G_Pin); osDelay(1); } /* USER CODE END 5 */ } /** * @brief Period elapsed callback in non blocking mode * @note This function is called when TIM6 interrupt took place, inside * HAL_TIM_IRQHandler(). It makes a direct call to HAL_IncTick() to increment * a global variable "uwTick" used as application time base. * @PAram htim : TIM handle * @retval None */ void HAL_TIM_PeriodElapsedCallback(TIM_HandleTypeDef *htim) { /* USER CODE BEGIN Callback 0 */ /* USER CODE END Callback 0 */ if (htim->Instance == TIM6) { HAL_IncTick(); } /* USER CODE BEGIN Callback 1 */ /* USER CODE END Callback 1 */ } /** * @brief This function is executed in case of error occurrence. * @retval None */ void Error_Handler(void) { /* USER CODE BEGIN Error_Handler_Debug */ /* User can add his own implementation to report the HAL error return state */ __disable_irq(); while (1) { } /* USER CODE END Error_Handler_Debug */ } #ifdef USE_FULL_ASSERT /** * @brief Reports the name of the source file and the source line number * where the assert_param error has occurred. * @PAram file: pointer to the source file name * @PAram line: assert_param error line source number * @retval None */ void assert_failed(uint8_t *file, uint32_t line) { /* USER CODE BEGIN 6 */ /* User can add his own implementation to report the file name and line number, ex: printf("Wrong parameters value: file %s on line %d\r\n", file, line) */ /* USER CODE END 6 */ } #endif /* USE_FULL_ASSERT */
View more

My assumption was that such a minimal example should work right off the bat but apparently that's not the case :)

Could someone point me at what I'm missing here please?

 

 

 

1 ACCEPTED SOLUTION

Accepted Solutions
vas
Associate II

This thread helped to solve the issue.

 

 

Temporary Solution: For those facing the same issue, add the following line to the User Code section in FreeRTOSConfig.h: /* USER CODE BEGIN Defines */ /* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */ #include CMSIS_device_header /* USER CODE END Defines */

 

View solution in original post

5 REPLIES 5
ahsrabrifat
Senior II

I think you need to disable WWDG in NVIC. 

I believe it's disabled

NVIC WWDG.png

I didn't touch any defaults.

vas
Associate II

I can't find SysTick_Handler implementation anywhere though. Neither in port.c, nor in stm32f0xx_it.c

When I implement an empty handler the execution constantly ends up in it. I am a novice at embedded programming but I feel like this might be the issue. Also I found this thread that can be related.

vas
Associate II

Should this be grayed out, and if not, how to fix that?

systick undefined.png

vas
Associate II

This thread helped to solve the issue.

 

 

Temporary Solution: For those facing the same issue, add the following line to the User Code section in FreeRTOSConfig.h: /* USER CODE BEGIN Defines */ /* Section where parameter definitions can be added (for instance, to override default ones in FreeRTOS.h) */ #include CMSIS_device_header /* USER CODE END Defines */